cancel
Showing results for 
Search instead for 
Did you mean: 

I wish for an upcomming ST event for forum moderators and contributors

T J
Lead
Posted on May 24, 2018 at 05:52

We would like to come meet in  France/Europe  maybe in Summer.

We would like to meet all the forum moderators and contributors and possibly book a day or two with the HAL engineers.

ST would hopefully be paying for the flights and accommodation for some of the more prolific contributors.

Then we will be able to work the timeline for the dual display, VR inspired wearable fanless ST-GPU launch.

I will bring the flowers.

1 ACCEPTED SOLUTION

Accepted Solutions
Posted on May 24, 2018 at 12:34

There was plenty to eat and drink ...

View solution in original post

8 REPLIES 8
T J
Lead
Posted on May 24, 2018 at 07:43

The flowers are for

st.mcu

ELMHIRI.Syrine

‌ and

DAHMEN.IMEN

‌ of course...

Amel NASRI
ST Employee
Posted on May 24, 2018 at 10:42

Hi T J,

Thanks for the flowers and the proposal.

May you explain more what do you expect from such event: the purpose, what to discuss? what to suggest? who do you suggest to be invited?...

I add

Kling.Brian

‌ in this discussion.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on May 24, 2018 at 11:42

Its an adventure.

Free Beer and pizzas for starters.. hehe

I would like to meet up with

meyer.frank

Neil.Andrew

garsi.khouloud

Waclawek.Jan

Turvey.Clive

oliverbeirne

and the crowd.

The group could discuss anything that anyone considers at length.

I am sure everyone has interesting projects to confab over if they want.

and we can give Clive the inaugural ST-Master Trophy, (we should decide on an Epic title for the trophy.)

It is interesting to me to see the future in 3D,

so I thought

if we are going to make an all new Fluid VR headset, then ST is going to need to know what we need to run it.

No one person can know everything about a product and foresee short comings.

Wearable, Fanless Dual 4k 100fps outputs feed into the VR screens.

Several ARM Cores and at least 16-1024 GPU cores, with 3D Audio Immersion.

H265 & WebGL are the primary mediums

Since we are making a new processor family, an optical port would give us TByte transfers with 1 or 2 pins

Embedded 1GByte Ram or Optical port Ram would be nice, while you are at it.

Easy enough to run 2x 4K screens over an Optical channel.

I thought optical would be beneficial in 2 ways.

Flexible / Wearable and distance is not an issue. (We need upto 3M at most) I guess

anyhow, my nuts and bolts aren't worked out, hence the need for befuddled conflaberations, pizza and flowers of course.

Posted on May 24, 2018 at 13:49

As Brian can no doubt recount, I've had this conversation with him where this is exactly not something I want to do.

http://www.google.com/search?q=busmans+holiday

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 24, 2018 at 12:10

Sounds like you're thinking of something like this: 

http://blog.antronics.co.uk/2014/06/26/didnt-we-have-a-loverly-time-the-days-we-went-to-paris/

  ?
Posted on May 24, 2018 at 12:28

Actually, I can't see any beer at that party. or pizzas or flowers.

You may understand that

Waclawek.Jan

‌,

meyer.frank

‌ , all of us really, we don't ask questions.

So its not about learning about ST.

Its about a support base get together and discuss anything you like.

I would like to suggest a new ST processor somewhat similar to the Tegra Pascal or at least like an Rk3399

if ST is listening or not.

Individually, it is beyond our dreams to make a new processor,

but since we support ST, maybe ST will want to move forward on a super scalar project as described by our team, or not.

but I did promise to bring flowers.

Posted on May 24, 2018 at 12:34

There was plenty to eat and drink ...

Posted on May 24, 2018 at 14:01

Neil.Andrew

said he would do Karaoke,

He sent me his video...