2022-05-23 2:28 AM
I am using the stm32h745ziq-nucleo board . I am generating the pulse in the cm7 and I am trying ton capture the falling edge of the pulse. I am getting the falling edge capture for every falling pulse But I want to capture only the 8th falling edge of that pulse.
What are the changes I want to make to get the 8th falling Edge capture.
Best Regards
sm.
2022-05-23 6:29 AM
Use another timer as a divider by 8. Than cascade two timers.
2022-05-23 8:31 AM
The TIM should have an Input Prescaler for the pins, although it won't let you pick particular pulses out of a train, it does permit measurement of period, over 1, 2, 4 or 8 pulses and that can be averaged
2022-05-23 10:49 PM
Hi @MasterT ,
Hi @Community member ,
I had gone through the reference manual But somewhere I am missing something ... If you send one example code base that would be great.
Regards
sm
2022-05-24 6:09 AM
After reading more replay, it;s not clear what is CM7 - another uCPU / board? Or it's the same, and you just routed signal to outside peripheral and need to get another synchronise pulse /8 ?.
For examples of code, get yourself stm32CubeMX software package installed, it includes bunch of projects for each board. I see InputCapture is missing in the stm32h745ziq subfolder, but you can study stm32h743 - should not be very different.