2022-03-28 3:08 AM
DMA config as below
hdma_tim.Instance = TIMx_CC1_DMA_INST;
hdma_tim.Init.Channel = DMA_CHANNEL_6;
hdma_tim.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_tim.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_tim.Init.MemInc = DMA_MINC_ENABLE;
hdma_tim.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
hdma_tim.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
hdma_tim.Init.Mode = DMA_CIRCULAR;
hdma_tim.Init.Priority = DMA_PRIORITY_HIGH;
hdma_tim.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
hdma_tim.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_tim.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_tim.Init.PeriphBurst = DMA_PBURST_SINGLE;
HAL_DMA_Init(&hdma_tim);
/* Link hdma_tim to hdma[TIM_DMA_ID_CC1] (channel1) */
__HAL_LINKDMA(&TIMx_handle, hdma[TIM_DMA_ID_CC1], hdma_tim);
/*##-2- Configure the NVIC for DMA #########################################*/
/* NVIC configuration for DMA transfer complete interrupt */
HAL_NVIC_SetPriority(TIMx_DMA_IRQn, 2, 4);
HAL_NVIC_EnableIRQ(TIMx_DMA_IRQn);
PWM generation code +++++++++++++++++++++++++++++++
TIMx_handle.Init.Period = 50;
TIMx_handle.Init.RepetitionCounter = 0;
TIMx_handle.Init.Prescaler = 0;
TIMx_handle.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
TIMx_handle.Init.CounterMode = TIM_COUNTERMODE_UP;
/*##-1- Initialize the timer in time base generation mode ##################*/
HAL_TIM_PWM_Init(&TIMx_handle);
/*##-2- Configure the PWM channels #########################################*/
/* Common configuration */
TIMx_sConfig.OCMode = TIM_OCMODE_PWM1;
TIMx_sConfig.OCPolarity = TIM_OCPOLARITY_HIGH;
TIMx_sConfig.Pulse = 5;//aCCValue_Buffer[0];
TIMx_sConfig.OCNPolarity = TIM_OCNPOLARITY_HIGH;
TIMx_sConfig.OCFastMode = TIM_OCFAST_DISABLE;
TIMx_sConfig.OCIdleState = TIM_OCIDLESTATE_RESET;
TIMx_sConfig.OCNIdleState = TIM_OCNIDLESTATE_RESET;
HAL_TIM_PWM_ConfigChannel(&TIMx_handle, &TIMx_sConfig, TIM_CHANNEL_1);
/*##-3- Start PWM signals generation #######################################*/
HAL_TIM_PWM_Start_DMA(&TIMx_handle, TIM_CHANNEL_1, aCCValue_Buffer, SIZEARRAY);
uint32_t aCCValue_Buffer[SIZEARRAY] = {0, 2, 4, 6, 8, 10, 12, 14, 16, 18, 20, 22, 24, 26, 28, 30, 32, 34, 36, 38, 40, 42, 44, 46, 48};
where SIZEARRAY is 25
Below image is for array size 10, came as expected
Below image is for array size 25, not good (I should see 25 different DCs)
2022-03-28 4:14 AM
Which STM32?
Read out and check/compare content of DMA (and perhaps also TIM) registers for both cases.
JW
2022-03-28 4:58 AM
Hi JW
Thanks for update
Am using STM32F427.
I want to update DutyCycle of a PWM timer at every 2us, so I made an array of 25 values and called
HAL_TIM_PWM_Start_DMA(&TIMx_handle, TIM_CHANNEL_1, aCCValue_Buffer, SIZEARRAY);
I have configurated DMA in circular mode.
According to my understanding I should get the below call back after full array gets updated.
void HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim)
{
HAL_TIM_PWM_Stop_DMA(&TIMx_handle, TIM_CHANNEL_1);
}
But this is not the case, each DU change this is getting called, is there any callback I get after full buffer is empty ?
Please help
2022-03-28 5:48 AM
> But this is not the case, each DU change this is getting called, is there any callback I get after full buffer is empty ?
I don't know, I don't use Cube.
Normally, interrupts from timer and from DMA have separate vectors, it's Cube which mingles them together.
JW