2021-03-28 03:04 AM
2021-03-28 03:14 AM
Check the continuity
Check signal with scope
2021-03-28 03:26 AM
Your STLink works. I have similar issue, on my L073 the StLink couldn't t connect. It was connecting and suddenly ST link interface stopped to work - on good few chips. St link was able to downlod the code in USART mode.
For me it is an issue with the chip - it is very sensitive.
Try following:
2021-03-28 08:08 AM
The CM0 parts want slower clocks on the SWD
2021-03-28 08:21 AM
2021-03-28 09:04 AM
... Check the continuity
It's ok.
... Check signal with scope
It seems that the MC is not responding in the second position of the breadboard.
first:second:
2021-03-28 09:06 AM
... Ensure you StLink works on some other device.
I tried another StLink, same behavior.
... Connect the uC via USART in boot mode.
I will try
2021-03-28 09:11 AM
2021-03-28 09:45 AM
2021-03-28 10:03 AM