cancel
Showing results for 
Search instead for 
Did you mean: 

I'm going crazy, look at the photos: if I move the SWD CLK connection in one point of the breadboard the connection works, in another it doesn't! The chip is a STM32L412KB, I tried to replace it but nothing! I also replaced the ST-LINK but nothing yet.

APast.1
Associate II

0693W000008y6ScQAI.jpg0693W000008y6SmQAI.jpg0693W000008y6SwQAI.jpg0693W000008y6T1QAI.jpg

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11

I'm not a fan of this type of bread-boarding, clearly have some signal integrity issue here. Keep things direct, with the minimum number of interconnects

Prefer wire-wrap or schmartboard-jumperwires here as these methods both have biting metal-to-metal connectivity.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
APast.1
Associate II

Thanks for your help, the only solution was to try and try to change the position of the connections until the error disappeared