cancel
Showing results for 
Search instead for 
Did you mean: 

I have a project using stm32f765,now i want to migrate to stm32H743.I want to know if i can use the code that has been written for stm32f765 instead of writing a new one, If yes , is it enough to only change the header files name?

FShak.1
Associate

Hi community. I mean for example are some changes necessary in some HAL or LL APIs for different peripherals or i should leave it as the way they were written in pervious code(Code for stm32F765) ?

1 REPLY 1
MM..1
Chief II

simple NO