cancel
Showing results for 
Search instead for 
Did you mean: 

I have a problem of using SPI in STM32H753VIT6 CHIP

KDG
Associate III

Hello,

I'm trying to do SPI communication with an ADE1201 chip through an STM32H753VIT6 chip.

The maximum allowed frequency of the ADE1201 is 10MHZ, so I set the SPI to communicate with the MCU at 6.25MHZ.

(The clock for SPI communication is 25MHZ, and I set the PRESCALER value to 4).

However, a strange phenomenon was observed.

화면 캡처 2024-01-31 133410.png

I observed through the scope that the SPI CS signal should be 0 continuously, but it turns to 1 in the middle.(See attached photo).

However, if I set the PRESCALER value to 8, the CS signal is continuously output as 0.

 

What could be the cause? And how can I solve this?

Could this be due to the usage of HAL_SPI_TransmitReceive function?

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Pierre_Paris
ST Employee

Hello @KDG ,

As I can see, here some remarks :

  • You declares NSSPMode to SPI_NSS_PULSE_ENABLE. This mode is activated by the SSOM bit in the SPIx_CR2 register. For SSOM = 1, SPI data frames are interleaved with SS non active pulses when MIDI[3:0]>1. That's explaining the behavior of your SPI4 CS line. According to RM0433, we are in a situation quite similar as shown in figure 620.Pierre_P_0-1706785910666.pngCan you change to SPI_NSS_PULSE_DISABLE ? Does that solve your issue ? 
  • It's recommended to set MasterKeepIOState to SPI_MASTER_KEEP_IO_STATE_ENABLE to avoid glitches.

Best Regards,

Pierre

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Pierre_Paris
ST Employee

Hello @KDG,

Thank you for your question !

Here some remark :

  • Can you share your code ? At least your SPI parameter configuration and what API you called (HAL_SPI_TransmitReceive, that's it?)
  • When prescaler = 8 (f = 3.12 MHz), the behavior is normal but when prescaler = 4 (f = 6.25MHz), there is sometimes the CS which turns to 1. This is the only change you made between both screen right ?
  • Also, do you have the values of registers ? SPI_CFG1 ? SPI_CFG2 (especially SSOE, SSOM & SSM) ? In master mode, the SS can be used either as an output or an input. As an input it can prevent a multi master bus collision, and as an output it can drive a slave select signal of a single slave. How many masters are on the bus ? 

Kind Regards,

Pierre

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks for the remark @Pierre_Paris 

 

These are the answers for your remarks

  • static void MX_SPI4_Init(void)
    {

    /* USER CODE BEGIN SPI4_Init 0 */

    /* USER CODE END SPI4_Init 0 */

    /* USER CODE BEGIN SPI4_Init 1 */

    /* USER CODE END SPI4_Init 1 */
    /* SPI4 parameter configuration*/
    hspi4.Instance = SPI4;
    hspi4.Init.Mode = SPI_MODE_MASTER;
    hspi4.Init.Direction = SPI_DIRECTION_2LINES;
    hspi4.Init.DataSize = SPI_DATASIZE_8BIT;
    hspi4.Init.CLKPolarity = SPI_POLARITY_HIGH;
    hspi4.Init.CLKPhase = SPI_PHASE_2EDGE;
    hspi4.Init.NSS = SPI_NSS_HARD_OUTPUT;
    hspi4.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4;
    hspi4.Init.FirstBit = SPI_FIRSTBIT_MSB;
    hspi4.Init.TIMode = SPI_TIMODE_DISABLE;
    hspi4.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
    hspi4.Init.CRCPolynomial = 0x0;
    hspi4.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
    hspi4.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
    hspi4.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
    hspi4.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
    hspi4.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
    hspi4.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
    hspi4.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
    hspi4.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
    hspi4.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
    hspi4.Init.IOSwap = SPI_IO_SWAP_DISABLE;
    if (HAL_SPI_Init(&hspi4) != HAL_OK)
    {
    Error_Handler();
    }
    /* USER CODE BEGIN SPI4_Init 2 */

    /* USER CODE END SPI4_Init 2 */

    }

    And the API IS
    HAL_SPI_TransmitReceive(&hspi4, u8_R_head_buffer, u8_R_buffer, 4 , 10 );
  • Yes, that is the only change made between both screeen

  • These are the values for the registers that you required
    • 화면 캡처 2024-02-01 093803.png

    • There are only one master on the bus 


I wonder if this would be enough for your remarks.

Thank you.

Sincerely,

KDG

Pierre_Paris
ST Employee

Hello @KDG ,

As I can see, here some remarks :

  • You declares NSSPMode to SPI_NSS_PULSE_ENABLE. This mode is activated by the SSOM bit in the SPIx_CR2 register. For SSOM = 1, SPI data frames are interleaved with SS non active pulses when MIDI[3:0]>1. That's explaining the behavior of your SPI4 CS line. According to RM0433, we are in a situation quite similar as shown in figure 620.Pierre_P_0-1706785910666.pngCan you change to SPI_NSS_PULSE_DISABLE ? Does that solve your issue ? 
  • It's recommended to set MasterKeepIOState to SPI_MASTER_KEEP_IO_STATE_ENABLE to avoid glitches.

Best Regards,

Pierre

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks @Pierre_Paris 

By your remarks, my problem is solved.