cancel
Showing results for 
Search instead for 
Did you mean: 

I cut the ST-LINK part, but there is no printf output on the serial monitor.

최민혁.1
Associate II

Hello?

I am a developer using the nucleo-f411re board.

I had a problem while trying to update the firmware by cutting the st-link part. The firmware is uploaded successfully, but the result of the printf function is not printed on the serial monitor.

Is there any other rule that says I have to remove sb or connect another line?

I connected the debugging port by referring to the link below.

https://community.openenergymonitor.org/t/stm32-hardware-development/7135/20

2 REPLIES 2

The UART doesn't connect via the SWD pins.​

RX and TX​ should be exposed on a second pair of pins.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Nikita91
Lead II

You have to connect the MCU UART pins to the CN3 connector of the st-link part.