2023-01-29 01:19 AM
STM32G030C8T6 has maximum critical crystal transconductance (gm) is 1.5 mA/V.
Crystal specifications that are mentioned in application note(page14) gmcrit = 0.23 mA/V with this gain margin > 5. But I checked many crystals datasheet but I am not able to find crystal with same specification.
Available crystals have greater ESR & Load capacitance which will lower the gain margin.
What should I do? Please help with the same.
2023-01-29 02:13 AM
HSE ... how MHz ?
2023-01-29 02:32 AM
8Mhz
2023-01-29 09:23 AM
any standard 8MHz crystal will work ;
or take a oscillator , not much more expensive today than crystal + 2x caps.