2020-02-07 5:52 AM
I have written ADC1_2_ IRQ Handler ISR and TIM2_IRQHandler. TIM2_IRQHandler is executed but ADC1_2_IRQHandler it is not executed.
I have also tried to trigger ADC1 injected group with JSWSTAR event and it works fine (ADC1_2_IRQHandler is executed).
The trouble exists booth whith simulator and with true hardware.
So I don't know why TIM2 CC1 event not work,
Thanks, following is my code (only initialization and ISR)
/*----------------------------------------------------------------------------
* Initialization function
*--------------------------------------------------------------------------*/
void initialize(void)
{
int index = 0;
/* - SYSCLK clock = 72 MHz
- HCLK clock (Core clock) = 72 MHz (AHB prescaler = /1)
- PCKL1 clock = 36 MHz (APB1 prescaler = /2 usato da TIM2 e PORT)
- PCKL2 clock = 72 MHz (APB2 prescaler = /1 usato da ADC2)
- TIM2CLK = 72 MHz
*/
/*----------------------------------------------------------------------------
* TIM2 configuration
*--------------------------------------------------------------------------*/
RCC->APB1ENR |= RCC_APB1ENR_TIM2EN;
/* Overflow frequency = TIM2CLK / ((TIM2_PSC + 1) * (TIM2_ARR + 1)).
At reset TIM2_PSC = 0.
If TIM2_ARR = 719 than
overflow frequency = TIM2CLK / ((TIM2_PSC + 1) * (TIM2_ARR + 1)) =
72 MHz / ((0 + 1) * (719 + 1)) = 100 kHz. */
TIM2->ARR = 719;
TIM2->CCR1 = TIM2->ARR;
TIM2->CCMR1 |= (0 * TIM_CCMR1_OC1M_2) | (0 * TIM_CCMR1_OC1M_1)
| (1 * TIM_CCMR1_OC1M_0);
TIM2->CR1 |= TIM_CR1_CEN;
TIM2->DIER |= TIM_DIER_CC1IE;
NVIC_EnableIRQ(TIM2_IRQn);
/*----------------------------------------------------------------------------
* PB1 as ADC_IN9 configuration
*--------------------------------------------------------------------------*/
RCC->APB2ENR |= RCC_APB2ENR_IOPBEN;
GPIOB->CRL |= (0 * GPIO_CRL_MODE1_1) | (0 * GPIO_CRL_MODE1_0);
GPIOB->CRL &= ~GPIO_CRL_CNF1;
GPIOB->CRL |= (0 * GPIO_CRL_CNF1_1) | (0 * GPIO_CRL_CNF1_0);
/*----------------------------------------------------------------------------
* PC4 as ADC_IN14 configuration
*--------------------------------------------------------------------------*/
RCC->APB2ENR |= RCC_APB2ENR_IOPCEN;
GPIOC->CRL |= (0 * GPIO_CRL_MODE4_1) | (0 * GPIO_CRL_MODE4_0);
GPIOC->CRL &= ~GPIO_CRL_CNF4;
GPIOC->CRL |= (0 * GPIO_CRL_CNF4_1) | (0 * GPIO_CRL_CNF4_0);
/*----------------------------------------------------------------------------
* ADC clock configuration
*--------------------------------------------------------------------------*/
/* ADCPRE = 10b ==> ADCCLK = PCLK2 / 6 = 72MHz / 6 = 12 MHz */
RCC->CFGR |= (1 * RCC_CFGR_ADCPRE_1) | (0 * RCC_CFGR_ADCPRE_0);
/*----------------------------------------------------------------------------
* ADC1 configuration
*--------------------------------------------------------------------------*/
RCC->APB2ENR |= RCC_APB2ENR_ADC1EN;
ADC1->JSQR |= (0 * ADC_JSQR_JL_1) | (1 * ADC_JSQR_JL_0);
ADC1->JSQR |= (0 * ADC_JSQR_JSQ3_4) | (1 * ADC_JSQR_JSQ3_3)
| (0 * ADC_JSQR_JSQ3_2) | (0 * ADC_JSQR_JSQ3_1)
| (1 * ADC_JSQR_JSQ3_0);
ADC1->JSQR |= (0 * ADC_JSQR_JSQ4_4) | (1 * ADC_JSQR_JSQ4_3)
| (1 * ADC_JSQR_JSQ4_2) | (1 * ADC_JSQR_JSQ4_1)
| (0 * ADC_JSQR_JSQ4_0);
ADC1->JOFR1 = (1UL << 11); /* 2^11 = 2048 */
ADC1->JOFR2 = (1UL << 11); /* 2^11 = 2048 */
ADC1->SMPR2 |= (0 * ADC_SMPR2_SMP9_2) | (0* ADC_SMPR2_SMP9_1)
| (0 * ADC_SMPR2_SMP9_0);
ADC1->SMPR1 |= (0 * ADC_SMPR1_SMP14_2) | (0* ADC_SMPR1_SMP14_1)
| (0 * ADC_SMPR1_SMP14_0);
ADC1->CR2 |= ADC_CR2_ADON;
/* This for cycle generates a delay greater than Tstab. From datasheet
Tstab max = 1 microsecond */
for (index = 0; index < 72; index++)
{
__NOP();
}
ADC1->CR1 |= ADC_CR1_JEOCIE;
ADC1->CR1 |= ADC_CR1_SCAN;
ADC1->CR2 |= ADC_CR2_JEXTTRIG;
ADC1->CR2 |= (0 * ADC_CR2_JEXTSEL_2) | (1 * ADC_CR2_JEXTSEL_1)
| (1 * ADC_CR2_JEXTSEL_0);
NVIC_EnableIRQ(ADC1_2_IRQn);
ADC1->CR2 |= ADC_CR2_CAL;
while(ADC1->CR2 & ADC_CR2_CAL)
{
}
}
/*------------------------------------------------------------------------------
ISR ADC
*----------------------------------------------------------------------------*/
volatile uint32_t counter_executions_ADC1_2_IRQHandler = 0;
void ADC1_2_IRQHandler(void)
{
ADC1->SR &= ~ADC_SR_JEOC;
counter_executions_ADC1_2_IRQHandler++;
}
/*------------------------------------------------------------------------------
ISR TIM2
*----------------------------------------------------------------------------*/
volatile uint32_t counter_executions_TIM2_IRQHandler = 0;
void TIM2_IRQHandler(void)
{
TIM2->SR &= ~TIM_SR_CC1IF;
counter_executions_TIM2_IRQHandler++;
}