2022-04-21 5:42 AM
2022-04-21 7:04 AM
2022-04-21 5:53 AM
Show your code. Are you waiting the required time before checking? Are you clearing DEEPPWD? Is the ADC clock enabled?
2022-04-21 5:59 AM
Why you are not following the section 26.4.6 of the reference manual?
2022-04-21 6:01 AM
I cleared DEEPPWD first line and I enabled all the clocks I could find (should the Domain register clock be enabled or enabling the clock assiociated to a peripheral enough). As for the waiting time the datasheet says to wait around 5µs I tried 10µs but shouldn't the LDORDY bit act as the delay check?
2022-04-21 6:01 AM
void ADC_Init(void) {
/***************REGISTER SHORTCUT*********************/
uint32_t ISR = *ADC_ISR;
uint32_t IER = *ADC_IER;
uint32_t CR = *ADC_CR;
uint32_t CFGR = *ADC_CFGR;
uint32_t CFGR2 = *ADC_CFGR2;
uint32_t SMPR1 = *ADC_SMPR1;
uint32_t PCSEL = *ADC_PCSEL;
uint32_t DR = *ADC_DR;
uint32_t DIFSEL = *ADC_DIFSEL;
uint32_t SQR1 = *ADC_SQR1;
uint32_t SQR2 = *ADC_SQR2;
uint32_t SQR3 = *ADC_SQR3;
uint32_t SQR4 = *ADC_SQR4;
uint32_t CSR = *ADC1_CSR;
uint32_t CCR = *ADC1_CCR;
/***************CLOCK and PIN config******************/
*RCC_APB4ENR|=(1 << SYSCFGEN);// Enable SYSCFG Peripheral Clock
*RCC_AHB4ENR |= (1 << GPIOAEN); //Enable clock GPIO port A
*GPIOA_MODER |= (3 << MODER0); //Analog mode port 0
*SYSCFG_PMCR|=(1 << PA0SO); //Connect the PA0 to PA0_C
*RCC_AHB1ENR |= (1 << ADC1EN); //ADC peripheral clock enable
/***************ADC not Enabled yet********************/
//ADC VOLTAGE REGULATOR-----------------------------
CR = 0x00000000; //End deep power down
*ADC_CR = CR;
CR = (1<<ADVREGEN); //ADC voltage regulator Enabled
*ADC_CR = CR;
while ((*ADC_ISR & (1 << LDORDY)) == 0) {
dataFromRegister=*ADC_ISR;
Serial.println(dataFromRegister,BIN);
}
//delayMicroseconds(10);//wait for voltage regulator to be enabled (datasheets quote 5µs delay)
//ADC CALIBRATION-----------------------------------
CR &= ~(1 << ADCALDIF);
*ADC_CR = CR;//ADCALDIF single ended inputs mode
CR = (1 << ADCALLIN); //ADCALLIN calibration linéaire ET offset
*ADC_CR = CR;
*ADC_CR |= (1 << ADCAL); //calibration ADCAL=1
while(*ADC_CR & (1 << ADCAL) != 0){}
//ADC prescaler selection clock and sample time delay
CCR |= (3<<CKMODE);
CCR |= (3<<PRESC);
CCR |= (8<<DELAY);
*ADC1_CCR = CCR;//
//Set input mode------------------------------------
DIFSEL &= ~(1 << DIFSEL1); //DIFSEL[19:0]: single ended mode for channel 1
*ADC_DIFSEL = DIFSEL;
/*******************ADC Enable**********************/
*ADC_ISR |= (1 << ADRDY); // Reset ADC ready flag
*ADC_CR |= (1 << ADEN); //Enable ADC
while (!(*ADC_ISR & (1 << ADRDY))); //Wait for ready flag
*ADC_ISR |= (1 << ADRDY);
/********************ADC Enabled********************/
//ADC CFGR------------------------------------------
CFGR |= (1 << OVRMOD); //OVRMOD = 1 DR overwritten if overrun
CFGR |= (6 << RES); //RES[2:0]: Data resolution 110=12bits
CFGR &= ~(3 << DMNGT); //DMNGT[1:0]: Data Management configuration 00 data stored in DR only
CFGR |= (1 << CONT); //CONT: Single / continuous conversion mode for regular conversions
CFGR &= ~(3 << EXTEN);//Hardware trigger detec disabled
*ADC_CFGR = CFGR;
//*ADC_CFGR2 |= (1 << 5);//right shift for oversampling
//ADC SQR1------------------------------------------
SQR1 |= (1 << SQ1); //1st conv chan 1 (00001) and one conv by sequence (0000)
*ADC_SQR1 = SQR1;
//ADC SMPR1-----------------------------------------
SMPR1 |= (3 << SMP1); //SMP0[2:0]: Channel 1 sampling time selection 011: 16.5 ADC clock cycles
*ADC_SMPR1 = SMPR1;
// ADC PCSEL----------------------------------------
PCSEL |= (1 << PCSEL1); //PCSEL[19:0] :Channel 1 (VINP[i]) pre selection
*ADC_PCSEL = PCSEL;
}
2022-04-21 6:05 AM
But I am, I have read it through and through looking for a missing step ...
2022-04-21 6:41 AM
Where is your definition of ADC_ISR? Is it volatile?
Using standard CMSIS headers would make things a lot easier for others to read.
When you debug the code, do you see the expected value within ADC_CR while waiting for LDORDY?
2022-04-21 6:51 AM
I define all of my registers this way :
volatile uint32_t* const REG = (uint32_t*) ADDRESS_HEXA;As for the second question weirdly enough I get a 100000000000000000000000000000 meaning DEEPPWD is still enabled (I must have made a dumb mistake somewhere)
2022-04-21 7:04 AM
2022-04-21 7:08 AM
It works thanks a lot!