2022-03-20 9:30 AM
The structure of the code is:
Application's memory map ("memory_map.ld"):
/* Common memory definition */
MEMORY
{
SHARED_RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 256
RAM (xrw) : ORIGIN = 0x20000100, LENGTH = 320K - LENGTH(SHARED_RAM)
BOOT_FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 32K
SLOT1_ROM (rx) : ORIGIN = 0x08008000, LENGTH = 360k
SLOT2_ROM (rx) : ORIGIN = 0x08062000, LENGTH = 360k
CLIENT_ROM (rx) : ORIGIN = 0x080BC000, LENGTH = 240k
SHARED_CFG (rx) : ORIGIN = 0x080F8000, LENGTH = 32k
}
/* SHARED_RAM is memory to pass messages between firmwares. Needs to hold data while MCU is not unpowered */
SECTIONS
{
.SHARED_RAM(NOLOAD) : {
KEEP(*(.SHARED_RAM))
} > SHARED_RAM
}
__sharedram_start__ = ORIGIN(SHARED_RAM);
__sharedram_size__ = LENGTH(SHARED_RAM);
__bootrom_start__ = ORIGIN(BOOT_FLASH);
__bootrom_size__ = LENGTH(BOOT_FLASH);
__slot1rom_start__ = ORIGIN(SLOT1_ROM);
__slot1rom_size__ = LENGTH(SLOT1_ROM);
__slot2rom_start__ = ORIGIN(SLOT2_ROM);
__slot2rom_size__ = LENGTH(SLOT2_ROM);
__clientrom_start__ = ORIGIN(CLIENT_ROM);
__clientrom_size__ = LENGTH(CLIENT_ROM);
/* offset to be used for locating the image header from start image address */
__fw_header_offset = 0x200;
/* offset to be used for locating firmware code (".text") after image header */
__fw_codestart_offset = 0x30;
/* bootloader configuration, stored at the last page of SHARED_CFG section */
__bootloader_cfg_addr = 0x080FF800;
Application's Flash linker scatter file:
INCLUDE memory_map.ld
/* Entry Point */
ENTRY(Reset_Handler)
/* Highest address of the user mode stack */
_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */
_Min_Heap_Size = 0x200 ; /* required amount of heap */
_Min_Stack_Size = 0x400 ; /* required amount of stack */
/* Sections */
SECTIONS
{
/* The Vector table into SLOT1_ROM Rom type memory */
.isr_vector : {
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} > SLOT1_ROM
/* The application image header */
.image_hdr : ALIGN(4) {
FILL(0xFF)
. = ORIGIN(SLOT1_ROM) + __fw_header_offset;
KEEP (*(.image_hdr))
} > SLOT1_ROM
/* The clientManiobra library image header */
CLIENT_HDR : ALIGN(4) {
FILL(0xFF)
. = __clientrom_start__;
KEEP (*(CLIENT_HDR))
} > CLIENT_ROM
/* The Client Library program code and other data into "CLIENT_ROM" slot in flash */
.text2 :
{
FILL(0xFF)
. = __clientrom_start__ + __fw_header_offset + __fw_codestart_offset;
. = ALIGN(4);
*clientManiobra.a:* (.text .text*) /* .text sections from Client Library (code) */
} > CLIENT_ROM
/* The program code and other data into "FLASH" Rom type memory */
.text : {
FILL(0xFF)
. = ORIGIN(SLOT1_ROM) + __fw_header_offset + __fw_codestart_offset;
. = ALIGN(4);
/* Before was: *(.text) */
/* Before was: *(.text*) */
*(EXCLUDE_FILE (*clientManiobra.a) .text .text*) /* .text sections (code) */
*(.glue_7)
*(.glue_7t)
*(.eh_frame) /* exception handling tables */
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
_etext = .; /* define a global symbols at end of code */
} > SLOT1_ROM
... (continues)...
Withing "clientManiobra" library code, the following code snippets are implemented:
typedef struct __attribute__((packed)) {
uint32_t magicWord;
uint16_t imageFormatVersion;
uint32_t crc;
uint32_t data_size;
uint8_t imageType;
uint16_t clientFamily;
uint8_t clientVersion;
f_init_TypeDef func_init; /* callbacks */
f_checkEndOfMsgCallback_TypeDef func_EndOfMsgCbk;
f_getCmdTypeDef func_getCmd;
f_getErrorTypeDef func_getError;
f_getRspTypeDef func_getRsp;
f_getUrcTypeDef func_getUrc;
f_extractElemTypeDef func_extractElem;
f_analyzeCmdTypeDef func_analyzeCmd;
f_analyzeParamTypeDef func_analyzeParam;
f_terminateCmdTypedef func_terminateCmd;
uint32_t reserved;
} client_image_hdr_t;
typedef void (*f_init_TypeDef)(uart_parser_context_t *p_upCtxt);
/* Global variables of clientManiobra */
static const client_image_hdr_t client_hdr __attribute__((section("CLIENT_HDR"))) = {
.magicWord = CLIENT_IMAGE_MAGIC,
.imageFormatVersion = CLIENT_IMAGE_CURRENT_VERSION,
.crc = 0, /* to be parsed in post-processing */
.data_size = 0x0000, /* to be parsed in post-processing */
.imageType = IMAGE_TYPE_CLIENT_LIBRARY,
.clientFamily = CLIENT_FAMILY_ORONA_ARCA,
.clientVersion = CLIENT_ORONA_FW_VERSION,
.func_init = &libInit,
.func_EndOfMsgCbk = &lib_checkEndOfMsgCallback,
.func_getCmd = &lib_getCmd,
.func_getError = &lib_getError,
.func_getRsp = &lib_getRsp,
.func_getUrc = &lib_getUrc,
.func_extractElem = &lib_extractElem,
.func_analyzeCmd = &lib_analyzeCmd,
.func_analyzeParam = &lib_analyzeParam,
.func_terminateCmd = &lib_terminateCmd,
.reserved = 0
};
All compiles perfect but linking is raising error.
It's already 3 days reviewing where may I be mistaken but no progress. Any help/suggestion will be highly appreciated.
Pol
Solved! Go to Solution.
2022-03-20 10:01 AM
How big is your .a file?
2022-03-20 9:51 AM
2022-03-20 10:01 AM
How big is your .a file?
2022-03-20 10:12 AM
upps, 1.303KB !! :frowning_face_with_open_mouth:
I was only focused on the header piece and didn't put attention on the overall library size...
Thanks for your feedback !!! I need to focus on the library size it is amazing big and it shoudn't...
Pol
2022-03-20 10:22 AM
from screen part .text 0x37b3C (222k OK) , but part .text2 is chaos...
2022-03-20 11:01 AM
I was able to fix clientManiobra.a size, now it is 45KB
Nevertheless the error still is reproducing....
make -j8 all
arm-none-eabi-gcc -o "Datalogger_DiscoL496_07.elf" @"objects.list" -mcpu=cortex-m4 -T"D:\LiftEye\devices\firmwares\ST\Datalogger_DiscoL496_07\STM32L496AGIX_FLASH.ld" --specs=nosys.specs -Wl,-Map="Datalogger_DiscoL496_07.map" -Wl,--gc-sections -static -L"D:\LiftEye\devices\firmwares\ST\Datalogger_DiscoL496_07" -L"D:\LiftEye\devices\firmwares\ST\libOronaArca\Debug" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
c:\st\stm32cubeide_1.0.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: Datalogger_DiscoL496_07.elf section `CLIENT_HDR' will not fit in region `CLIENT_ROM'
c:\st\stm32cubeide_1.0.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: region `CLIENT_ROM' overflowed by 269730352 bytes
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:84: Datalogger_DiscoL496_07.elf] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.
18:44:50 Build Failed. 3 errors, 0 warnings. (took 2s.621ms)
Having a look at generated .map file:
.SHARED_RAM
*(.SHARED_RAM)
0x0000000020000000 __sharedram_start__ = ORIGIN (SHARED_RAM)
0x0000000000000100 __sharedram_size__ = LENGTH (SHARED_RAM)
0x0000000008000000 __bootrom_start__ = ORIGIN (BOOT_FLASH)
0x0000000000008000 __bootrom_size__ = LENGTH (BOOT_FLASH)
0x0000000008008000 __slot1rom_start__ = ORIGIN (SLOT1_ROM)
0x000000000005a000 __slot1rom_size__ = LENGTH (SLOT1_ROM)
0x0000000008062000 __slot2rom_start__ = ORIGIN (SLOT2_ROM)
0x000000000005a000 __slot2rom_size__ = LENGTH (SLOT2_ROM)
0x00000000080bc000 __clientrom_start__ = ORIGIN (CLIENT_ROM)
0x000000000003c000 __clientrom_size__ = LENGTH (CLIENT_ROM)
0x0000000000000200 __fw_header_offset = 0x200
0x0000000000000030 __fw_codestart_offset = 0x30
0x00000000080ff800 __bootloader_cfg_addr = 0x80ff800
0x0000000020050000 _estack = (ORIGIN (RAM) + LENGTH (RAM))
0x0000000000000200 _Min_Heap_Size = 0x200
0x0000000000000400 _Min_Stack_Size = 0x400
.isr_vector 0x0000000008008000 0x1ac
0x0000000008008000 . = ALIGN (0x4)
*(.isr_vector)
.isr_vector 0x0000000008008000 0x1ac ./Core/Startup/startup_stm32l496agix.o
0x0000000008008000 g_pfnVectors
0x00000000080081ac . = ALIGN (0x4)
.image_hdr 0x00000000080081ac 0x70
FILL mask 0xff
0x0000000008008200 . = (ORIGIN (SLOT1_ROM) + __fw_header_offset)
*fill* 0x00000000080081ac 0x54 ff
*(.image_hdr)
.image_hdr 0x0000000008008200 0x1c ./App/Device_Core/app_device_logic.o
CLIENT_HDR 0x00000000080bc000 0x80bc000
FILL mask 0xff
0x00000000080bc000 . = __clientrom_start__
*fill* 0x00000000080bc000 0x80bc000 ff
*(CLIENT_HDR)
.text2 0x0000000010178000 0x80bc230
FILL mask 0xff
0x00000000080bc230 . = ((__clientrom_start__ + __fw_header_offset) + __fw_codestart_offset)
*fill* 0x0000000010178000 0x80bc230 ff
0x0000000018234230 . = ALIGN (0x4)
*clientManiobra.a:*(.text .text*)
.text 0x0000000008008220 0x37b3c
FILL mask 0xff
0x0000000008008230 . = ((ORIGIN (SLOT1_ROM) + __fw_header_offset) + __fw_codestart_offset)
*fill* 0x0000000008008220 0x10 ff
0x0000000008008230 . = ALIGN (0x4)
*(EXCLUDE_FILE(*clientManiobra.a) .text .text*)
.text 0x0000000008008230 0x40 c:/st/stm32cubeide_1.0.1/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346/tools/bin/../lib/gcc/arm-none-eabi/9.3.1/thumb/v7e-m+fp/hard/crtbegin.o
.text.AT_init 0x0000000008008270 0x130 ./App/Cellular/Cellular_Core/AT_Core/at_core.o
0x0000000008008270 AT_init
.text.AT_open 0x00000000080083a0 0x210 ./App/Cellular/Cellular_Core/AT_Core/at_core.o
0x00000000080083a0 AT_open
.text.AT_open_channel
0x00000000080085b0 0x1b4 ./App/Cellular/Cellular_Core/AT_Core/at_core.o
0x00000000080085b0 AT_open_channel
... etc....
In row 34, the provided size in the map file for section CLIENT_HDR is 0x80bc000 !!
Any hints will be very much appreciated.