cancel
Showing results for 
Search instead for 
Did you mean: 

i am sanding data too my serial monitor to uart2 and uart to data transmit and received and transmit to uart6 and uart 6 received and and transmit back my serial monitor plz help i am working stm32f411vet6 microcontroler

kjosh.1
Associate II
 
17 REPLIES 17

Is there a question?

JW

kjosh.1
Associate II

i am sanding data my serial monitor to uart2 ,uart2 received data and transmit to uart6 ,uart6 received data and transmit back to serial monitor with stm32f411 microcontroller plz give me answer

yes

i am sanding data my serial monitor to uart2 ,uart2 received data and transmit to uart6 ,uart6 received data and transmit back to serial monitor with stm32f411 microcontroller plz give me answer

Repeating the same information is not going to move this forward. When prompted like this it means your question lacks structure or detail

What isn't working?

Show initialization code, clocks, pins, etc

Show code that doing the interaction

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

You want code showing forwarding back and forth between UART2 <-> UART6 ?

What board are you using?

Which pins are connected to the UARTs ?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
kjosh.1
Associate II

stm32f411vet6 microcontroller using

kjosh.1
Associate II

and i am using mx 32 cube id and using hadware bord uart2 and uart6 and yp-05 card using one card using to uart2 and one is using for uart6

So this YP-05, that's some USB-to-CMOS dongle?

You still haven't asked a question, you keep make statements.

What do you want people here to do?

Write the code for you?

Figure out what pins you're using?

Find some UART examples for your board or the F4 generally, adapt.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..