cancel
Showing results for 
Search instead for 
Did you mean: 

How to wake up from stop mode with alarm A?

Emm1592
Associate II

Hello,

I'm trying to wake up from stop 1 with the alarm A, and I was wondering if someone can help me with this.

Here is my code (I'm using HAL libraries first, the "easy" way base on the example ST gives: PWR/STOP1_RTC):

...

int main(void){

GPIO_InitTypeDef GPIO_InitStruct;

 HAL_Init();

BSP_LED_Init(LED2); 

SystemClock_Config(); //Config RCC

__HAL_RCC_PWR_CLK_ENABLE();

  __HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_MSI);

SystemPower_Config(); //Config the RTC ----> 19:50:00

setAlarmA(); // The alarm is set to: 19:51:00

while(1){

...

  /* Disable all used wakeup source */

HAL_RTCEx_DeactivateWakeUpTimer(&RTCHandle);

/* Re-enable wakeup source */

HAL_RTCEx_SetWakeUpTimer_IT( ........?........);

/* Enter STOP 1 mode */

 HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);

} //End while (1)

} // End main

I don't know how to tell my STM that it will be woken up by the Alarm A (It goes there in the line I highlighted?) How do I do that?

My idea is to wake up the system at 19:51:00 and re-set the alarm A to: 19:52:00. In the alarmA callback, I wrote the following:

void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc){

setNewAlarmA();

}

I'm using the Nucleo Board STM32L476RG

Thank you very much for all the help.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Jack Peacock_2
Senior III

RTC Alarm is not a timer per se. Alarm A/B uses the RTC EXTI18 external interrupt, so EXTI18 must be enabled on rising edge to wake from STOP mode, for the NVIC vector in the configuration. Don't use the HAL, no idea how it handles EXTIs, but I use alarm B for something similar. RTC must be running in STOP mode with LSE or LSI clock on.

Jack Peacock