2020-04-23 04:05 AM
Due to few requirements i am required to use FW 1.24.0 as the firmware package.How can i make the change in CUBEMX project management settings .Kindly help
2020-04-23 06:22 AM
Hello,
Please refer to the User manual of STM32CubeMX: UM1718
you will find the description needed in page 128 :
Firmware location selection option:
The default location is the location specified under the Help > updater settings menu. Deselecting the Use Default Firmware Location checkbox allows the user to specify a different path for the firmware that will be used for the project.
Please see the Figure 104.
Regards