cancel
Showing results for 
Search instead for 
Did you mean: 

How to use STM32CubeProgrammer and the STLINK-V3SET to program STM32G431C8U6 UFQFPN48 chip

ektan
Associate

Dear All,

I have the STM32G431C8U6 UFQFPN48 chip mounted on the breakout board (QFPN48 to DIP48). 

How to use STM32CubeProgrammer and the STLINK-V3SET to program the STM32G431C8U6 UFQFPN48 chip on the breakout board?

 

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions

Make sure the G4 is properly powered. Both digital and analogue supplies. Capacitors on VCAP pins if present.

Connect VCC-TARGET, GND, NRST, SWDIO and SWCLK to the ST-LINK/V3

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2

Make sure the G4 is properly powered. Both digital and analogue supplies. Capacitors on VCAP pins if present.

Connect VCC-TARGET, GND, NRST, SWDIO and SWCLK to the ST-LINK/V3

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi Tesla DeLorean,

Please confirm the pins below are correct as stated.

NRST - pin 7

SWDIO - pin 36

SWCLK - pin 37

VDD - pin 21, 23, 35, and 48

GND - Exposed pad

Thank you.