2023-10-15 05:08 PM
Dear All,
I have the STM32G431C8U6 UFQFPN48 chip mounted on the breakout board (QFPN48 to DIP48).
How to use STM32CubeProgrammer and the STLINK-V3SET to program the STM32G431C8U6 UFQFPN48 chip on the breakout board?
Thank you.
Solved! Go to Solution.
2023-10-15 05:41 PM
Make sure the G4 is properly powered. Both digital and analogue supplies. Capacitors on VCAP pins if present.
Connect VCC-TARGET, GND, NRST, SWDIO and SWCLK to the ST-LINK/V3
2023-10-15 05:41 PM
Make sure the G4 is properly powered. Both digital and analogue supplies. Capacitors on VCAP pins if present.
Connect VCC-TARGET, GND, NRST, SWDIO and SWCLK to the ST-LINK/V3
2023-10-22 09:13 PM
Hi Tesla DeLorean,
Please confirm the pins below are correct as stated.
NRST - pin 7
SWDIO - pin 36
SWCLK - pin 37
VDD - pin 21, 23, 35, and 48
GND - Exposed pad
Thank you.