2020-10-10 10:19 AM
I've been trying to get Oversampling working using polling for ADC completion, but I'm not seeing the expected results. I found one example for x4 oversampling, but in reality that doesn't seem to actually be doing anything. I am trying to use 32 for the ratio using the appropriate definition from the include file. But when I do that I wind up with a value that is about one fourth what it should be. So I'm looking for a working example of oversampling with this processor.
Thanks,
2020-10-13 7:58 AM
2020-10-13 8:24 AM
Thanks for the pointer to the example. When I attempted to use the oversampling configuration I was not getting correct results. Digging into the specs for the 753 MCU we are using I was able to resolve the issue and now get consistent results, and within the expected tolerance for the voltage that is being monitored.