2017-06-09 7:51 AM
Hi,
I am new to STM32 MCUs and looking for a simple tutorial on how to upload software to this board.
Of course I checked google etc beforehand but have not found a simple tutorial on how to get the B-L072Z-LRWAN1 started (normally I am using platformIO but open for other suggestions to easily get STM discovery board up and running).
Any help or guidance would be appreciated :)
2017-06-09 7:59 AM
Hi
debuffel
,You have in the
/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fst_com%2Fen%2Fproducts%2Fevaluation-tools%2Fproduct-evaluation-tools%2Fmcu-eval-tools%2Fstm32-mcu-eval-tools%2Fstm32-mcu-discovery-kits%2Fb-l072z-lrwan1.html
page User manuals and a link to the software expansion for STM32Cube with UM2073 user manual.Hope this helps you.
Regards
Imen
2017-06-09 8:12 AM
The ST-LINK Utilities can download .HEX or .BIN files.
Integrated directly into tools like Keil, basically open the project, select the target, build, download, done.
2017-06-09 10:19 AM
Thanks Imen. I already downloaded these sw packages // however once downloaded there is not a document which explains how to use files (probably for the novice it goes without saying ... not for me (yet)). That's why I was looking for simple tutorial movie or doc.
2017-06-09 10:20 AM
Thanks. Maybe I need to use Keil / and what is the function of icube sw in that case?
2017-06-09 2:28 PM
Keil looks ok - but to build sw for the STM32L072 Discovery Kit it seems that I need the another (commercial) version of Keil.
linking...
.\mlm32l07x01\NUCLEO_CUBE_LORA.axf: error: L6050U: The code size of this image (40116 bytes) exceeds the maximum allowed for this version of the linker.Finished: 0 information, 0 warning, 0 error and 1 fatal error messages.'.\mlm32l07x01\NUCLEO_CUBE_LORA.axf' - 1 Error(s), 0 Warning(s).Target not created.Build Time Elapsed: 00:00:06I thought discovery kits should be easy ???? ;)
2017-06-10 11:42 AM
http://www2.keil.com/stmicroelectronics-stm32/mdk
2017-06-12 1:08 AM
Thanks a lot for the tips Clive. Got the disco working!