2021-03-06 10:24 PM
Hello!
I have STM32H743B
I configure TIM4 to PWM GEneration
static void MX_TIM4_Init(void)
{
/* USER CODE BEGIN TIM4_Init 0 */
/* USER CODE END TIM4_Init 0 */
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
/* USER CODE BEGIN TIM4_Init 1 */
/* USER CODE END TIM4_Init 1 */
htim4.Instance = TIM4;
htim4.Init.Prescaler = 0;
htim4.Init.CounterMode = TIM_COUNTERMODE_UP;
htim4.Init.Period = 65535;
htim4.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim4.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_PWM_Init(&htim4) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim4, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 0xFFFF;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_PWM_ConfigChannel(&htim4, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM4_Init 2 */
/* USER CODE END TIM4_Init 2 */
HAL_TIM_MspPostInit(&htim4);
}I try to change duty cycle
void SetBacklightBrightness(uint16_t brightness)
{
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = brightness<<8;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_PWM_ConfigChannel(&htim4, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
{
Error_Handler();
}
} but duty cycle not updates...
How to solve this problem?
Solved! Go to Solution.
2021-03-06 11:04 PM
I found solution.
function HAL_TIM_PWM_ConfigChannel resets CCER register.
After adding to code "TIM4->CCER=0x00000010;" problem was solved.
Thanks!
2021-03-06 11:01 PM
There is a HAL macro __HAL_TIM_SET_COMPARE just for changing that single register. Not tried on H7 though.
hth
KnarfB
2021-03-06 11:04 PM
I found solution.
function HAL_TIM_PWM_ConfigChannel resets CCER register.
After adding to code "TIM4->CCER=0x00000010;" problem was solved.
Thanks!
2021-03-06 11:18 PM
I use for change directly for example
TIM4->CCR2+=50;