2023-01-08 6:29 PM
I have successfully transmit and received data using CAN1. But having problem with CAN2.
I have go through all the configuration to enable the CAN2 however, I unable to transmit the data through CAN2.
What I have done:
1) Enable CAN2 ( PB12 [Rx], PB13 [Tx] )
2) Configure the Clock, HSE Crystal 8Mhz
3) Configure the bitrate to 500kbps
4) Enable CAN2 RX0 interrupts and CAN2 RX1 interrupt
5) For CAN1, canfilter.FilterActivation = ENABLE; canfilter.FilterBank = 0; and canfilter.SlaveStartFilterBank = 14;
6) For CAN2, canfilter2.FilterActivation = ENABLE; canfilter2.FilterBank = 14; and canfilter2.SlaveStartFilterBank = 14;
7) I have check all the hardware is OK, all are connected.
Behaviour
1) CAN1 is able to transmit and received data successfully
2) CAN2 fail to transmit or received data.
The Code
====================================================
/* USER CODE BEGIN 0 */
// Configure for CAN1
CAN_RxHeaderTypeDef RxHeader; //CAN Bus Receiver Header
CAN_TxHeaderTypeDef TxHeader; //CAN Bus Transmit Header
uint32_t TxMailbox; //CAN Bus Mail box variable
uint8_t RxData[8] = {0,0,0,0,0,0,0,0}; //CAN Bus Receive Buffer
uint8_t TxData[8] = {0,0,0,0,0,0,0,0}; //CAN Bus Transmit Buffer
HAL_StatusTypeDef status_can1;
uint8_t heartbeat = 0;
// Configure for CAN2
CAN_RxHeaderTypeDef RxHeader2; //CAN2 Bus Receiver Header
CAN_TxHeaderTypeDef TxHeader2; //CAN2 Bus Transmit Header
uint32_t TxMailbox2; //CAN2 Bus Mail box variable
uint8_t RxData2[8] = {0,0,0,0,0,0,0,0}; //CAN2 Bus Receive Buffer
uint8_t TxData2[8] = {0,0,0,0,0,0,0,0}; //CAN2 Bus Transmit Buffer
HAL_StatusTypeDef status_can2;
/* USER CODE END 0 */
/* USER CODE BEGIN 2 */
//Start CAN1
HAL_CAN_Start(&hcan1);
//Activate CAN received notification
HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING);
TxHeader.DLC = 2; //Send 2 byte of data
TxHeader.ExtId = 0;
TxHeader.IDE = CAN_ID_STD;
TxHeader.RTR = CAN_RTR_DATA;
TxHeader.StdId = 0x304; //Can ID
TxHeader.TransmitGlobalTime = DISABLE;
//Start CAN2
if(HAL_CAN_Start(&hcan2) == HAL_OK)
{
uint8_t hal_ok[14] = ">2 Start_OK\r\n";
HAL_UART_Transmit(&huart1, hal_ok, 13, 50);
}
//Activate CAN received notification
if(HAL_CAN_ActivateNotification(&hcan2, CAN_IT_RX_FIFO1_MSG_PENDING) == HAL_OK)
{
uint8_t hal_ok[12] = ">2 Noti_OK\r\n";
HAL_UART_Transmit(&huart1, hal_ok, 12, 50);
}
TxHeader2.DLC = 2; //Send 2 byte of data
TxHeader2.ExtId = 0;
TxHeader2.IDE = CAN_ID_STD;
TxHeader2.RTR = CAN_RTR_DATA;
TxHeader2.StdId = 0x504; //Can ID
TxHeader2.TransmitGlobalTime = DISABLE;
/* USER CODE END 2 */
/* USER CODE BEGIN 3 */
heartbeat++;
TxData2[0] = heartbeat;
TxData2[1] = 0x00;
status_can2 = HAL_CAN_AddTxMessage(&hcan2, &TxHeader2, TxData2, &TxMailbox);
if(status_can2 == HAL_OK)
{
uint8_t hal_ok[11] = ">2 HAL_OK\r\n";
HAL_UART_Transmit(&huart1, hal_ok, 11, 50);
}
else if(status_can2 == HAL_ERROR)
{
uint8_t hal_error[14] = ">2 HAL_ERROR\r\n";
HAL_UART_Transmit(&huart1, hal_error, 14, 50);
}
else if(status_can2 == HAL_BUSY)
{
uint8_t hal_busy[13] = ">2 HAL_BUSY\r\n";
HAL_UART_Transmit(&huart1, hal_busy, 13, 50);
}
else if(status_can2 == HAL_TIMEOUT)
{
uint8_t hal_timeout[16] = ">2 HAL_TIMEOUT\r\n";
HAL_UART_Transmit(&huart1, hal_timeout, 16, 50);
}
else
{
uint8_t _message[12] = ">2 NOTHING\r\n";
HAL_UART_Transmit(&huart1, _message, 12, 50);
}
//6) Toggle LED
HAL_Delay(1000);
}
/* USER CODE END 3 */
static void MX_CAN1_Init(void)
{
/* USER CODE BEGIN CAN1_Init 0 */
/* USER CODE END CAN1_Init 0 */
/* USER CODE BEGIN CAN1_Init 1 */
/* USER CODE END CAN1_Init 1 */
hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 18;
hcan1.Init.Mode = CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeSeg1 = CAN_BS1_2TQ;
hcan1.Init.TimeSeg2 = CAN_BS2_1TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = DISABLE;
hcan1.Init.AutoWakeUp = DISABLE;
hcan1.Init.AutoRetransmission = DISABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN1_Init 2 */
CAN_FilterTypeDef canfilter; //CAN Filter configuration
canfilter.FilterActivation = ENABLE;
canfilter.FilterBank = 0;
canfilter.FilterFIFOAssignment = CAN_RX_FIFO0;
canfilter.FilterIdHigh = 0x203<<5;
canfilter.FilterIdLow = 0;
canfilter.FilterMaskIdHigh = 0x203<<5;
canfilter.FilterMaskIdLow = 0;
canfilter.FilterMode = CAN_FILTERMODE_IDMASK;
canfilter.FilterScale = CAN_FILTERSCALE_32BIT;
canfilter.SlaveStartFilterBank = 14; //Slave Filter bank start at 14 to 28
HAL_CAN_ConfigFilter(&hcan1,&canfilter);
/* USER CODE END CAN1_Init 2 */
}
static void MX_CAN2_Init(void)
{
/* USER CODE BEGIN CAN2_Init 0 */
/* USER CODE END CAN2_Init 0 */
/* USER CODE BEGIN CAN2_Init 1 */
/* USER CODE END CAN2_Init 1 */
hcan2.Instance = CAN2;
hcan2.Init.Prescaler = 18;
hcan2.Init.Mode = CAN_MODE_NORMAL;
hcan2.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan2.Init.TimeSeg1 = CAN_BS1_1TQ;
hcan2.Init.TimeSeg2 = CAN_BS2_2TQ;
hcan2.Init.TimeTriggeredMode = DISABLE;
hcan2.Init.AutoBusOff = DISABLE;
hcan2.Init.AutoWakeUp = DISABLE;
hcan2.Init.AutoRetransmission = DISABLE;
hcan2.Init.ReceiveFifoLocked = DISABLE;
hcan2.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN2_Init 2 */
CAN_FilterTypeDef canfilter2; //CAN Filter configuration
canfilter2.FilterActivation = ENABLE;
canfilter2.FilterBank = 14;
canfilter2.FilterFIFOAssignment = CAN_RX_FIFO1;
canfilter2.FilterIdHigh = 0x0000;
canfilter2.FilterIdLow = 0x0000;
canfilter2.FilterMaskIdHigh = 0x0000;
canfilter2.FilterMaskIdLow = 0x0000;
canfilter2.FilterMode = CAN_FILTERMODE_IDMASK;
canfilter2.FilterScale = CAN_FILTERSCALE_32BIT;
canfilter2.SlaveStartFilterBank = 14; //Slave Filter bank start at 14 to 28
if(HAL_CAN_ConfigFilter(&hcan2,&canfilter2) == HAL_OK)
{
uint8_t hal_ok[14] = ">2 Filter_OK\r\n";
HAL_UART_Transmit(&huart1, hal_ok, 14, 50);
}
/* USER CODE END CAN2_Init 2 */
}
/* USER CODE BEGIN 4 */
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
//Received CAN data
if (HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
{
Error_Handler();
}
//Feedback through CAN1
//Send to serial
uint8_t _msg_can[22] = ">> IPC CAN Receiving\r\n";
HAL_UART_Transmit(&huart1, _msg_can, 22, 50);
}
void HAL_CAN_RxFifo1MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
//Received CAN data
if (HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO1, &RxHeader2, RxData2) != HAL_OK)
{
Error_Handler();
}
//Feedback through CAN1
//Send to serial
uint8_t _msg_can[22] = ">> DBW CAN Receiving\r\n";
HAL_UART_Transmit(&huart1, _msg_can, 22, 50);
}
/* USER CODE END 4 */
2023-01-08 9:07 PM
It's difficult to read your code as is. You need to post your code as a code snippet.
2023-01-08 9:11 PM
@Community member thanks. I have edit it. Do u have any idea for me to troubleshoot the CAN2 problem on STM32?
2023-01-09 11:53 PM
Do you see your uart message when you call HAL_CAN_Start(&hcan2) ?
//Start CAN2
if(HAL_CAN_Start(&hcan2) == HAL_OK)
{
uint8_t hal_ok[14] = ">2 Start_OK\r\n";
HAL_UART_Transmit(&huart1, hal_ok, 13, 50);
}
2023-01-12 11:49 PM
">2 Start_OK"
I have validate the following
HAL_CAN_Init for CAN1 : HAL_OK
HAL_CAN_Init for CAN2 : HAL_OK
HAL_CAN_ConfigFilter for CAN1 : HAL_OK
HAL_CAN_ConfigFilter for CAN2 : HAL_OK
HAL_CAN_Start for CAN1 : HAL_OK
HAL_CAN_Start for CAN2 : HAL_OK
HAL_CAN_ActivateNotification for CAN1 : HAL_OK
HAL_CAN_AddTxMessage for CAN1 : HAL_OK
HAL_CAN_ActivateNotification for CAN2 : HAL_OK
HAL_CAN_AddTxMessage for CAN2 : HAL_OK
but the CAN2 does not transmit any data to PEAK CAN View
After a while, the CAN2 becomes HAL_ERROR
2023-06-02 6:42 AM
Any answer to above questions ? Or still they are working on it ?