cancel
Showing results for 
Search instead for 
Did you mean: 

How to translate this DMA configuration from a PSoC device to a STM32

xpp07
Senior

The code below was implemented using a PsoC device. Maybe someone here can help me understand it and do the same in a STM32 device. AFAIK, the code is intended to build a quad buffer, but I don't understand how this is being implemented within a single array. I'm using STM32G0 and I have tested the ADC channel and DMA circular mode with HT and TC interrupts using HAL and it works OK.

Below the DMA configuration in the Psoc device:

void DMA1_Config(void)
{
    uint8 DMA1_Chan;
    uint8 DMA1_TD[4];
    
    #define TRANSFER_COUNT          (NO_SAMPLES * 2)    
    #define BUFFER_1                (NO_SAMPLES)
    #define BUFFER_2                (NO_SAMPLES * 2)
    #define BUFFER_3                (NO_SAMPLES * 3)
 
    #define DMA_BYTES_PER_BURST     (2u)
    #define DMA_REQUEST_PER_BURST   (1u)
    #define DMA_SRC_BASE            (CYDEV_PERIPH_BASE)
    #define DMA_DST_BASE            (CYDEV_SRAM_BASE)
 
	DMA1_Chan = DMA1_DmaInitialize(DMA_BYTES_PER_BURST, DMA_REQUEST_PER_BURST, HI16(DMA_SRC_BASE), HI16(DMA_DST_BASE));
	DMA1_TD[0] = CyDmaTdAllocate();
	DMA1_TD[1] = CyDmaTdAllocate();
	DMA1_TD[2] = CyDmaTdAllocate();
	DMA1_TD[3] = CyDmaTdAllocate();
    
    CyDmaTdSetConfiguration(DMA1_TD[0], TRANSFER_COUNT, DMA1_TD[1], DMA1__TD_TERMOUT_EN | TD_INC_DST_ADR);   
 	CyDmaTdSetConfiguration(DMA1_TD[1], TRANSFER_COUNT, DMA1_TD[2], DMA1__TD_TERMOUT_EN | TD_INC_DST_ADR);
    CyDmaTdSetConfiguration(DMA1_TD[2], TRANSFER_COUNT, DMA1_TD[3], DMA1__TD_TERMOUT_EN | TD_INC_DST_ADR);   
 	CyDmaTdSetConfiguration(DMA1_TD[3], TRANSFER_COUNT, DMA1_TD[0], DMA1__TD_TERMOUT_EN | TD_INC_DST_ADR);
    
    // Target 
    CyDmaTdSetAddress(DMA1_TD[0], LO16((uint32)ADC_1_DEC_SAMP_PTR), LO16((uint32)(&Buffer[0])));
    CyDmaTdSetAddress(DMA1_TD[1], LO16((uint32)ADC_1_DEC_SAMP_PTR), LO16((uint32)(&Buffer[BUFFER_1])));
    CyDmaTdSetAddress(DMA1_TD[2], LO16((uint32)ADC_1_DEC_SAMP_PTR), LO16((uint32)(&Buffer[BUFFER_2]))); 
    CyDmaTdSetAddress(DMA1_TD[3], LO16((uint32)ADC_1_DEC_SAMP_PTR), LO16((uint32)(&Buffer[BUFFER_3]))); 
 
	CyDmaChSetInitialTd(DMA1_Chan, DMA1_TD[0]);
	CyDmaChEnable(DMA1_Chan, 1);// Enable DMA channel
}

This is how the buffer is used within a function. This function is called every time 1/4 buffer fill interrupt:

#define NO_SAMPLES 200u             // number of samples to acquire (1/4 buffer)
 
int16 Buffer[4 * NO_SAMPLES];     
 
uint8 Window[NO_SAMPLES];         
 
double RMS_find() 
{
    uint64 AccMS64 = 0;                     
    uint16 offset1=0, offset2=0;            
    uint16 i;
    int16 v;
   
    switch (BufferSection)
    {
        case 0: // -->0..1..2--3
                offset1 = 3 * NO_SAMPLES;
                offset2 = 0;
                BufferSection=1;            // next section
                break;
                
        case 1: // --0-->1..2..3
                offset1 = 0;
                offset2 = NO_SAMPLES;
                BufferSection=2;            // next section
                break;
                
        case 2: // ..0--1-->2..3
                offset1 = NO_SAMPLES;
                offset2 = 2 * NO_SAMPLES;
                BufferSection=3;            // next section
                break;
                
        case 3: // ..0..1--2-->3
                offset1 = 2 * NO_SAMPLES;
                offset2 = 3 * NO_SAMPLES;
                BufferSection=0;            // next section
                break;
    
        default:                            // should not come here
                BufferSection=0;                            
    } 
    
    for( i=0; i<NO_SAMPLES; i++) {                          
        v = Buffer[i+offset1];                              
        AccMS64 +=  (uint64)(v*v) * Window[(NO_SAMPLES-1)-i];  
    }
 
    for( i=0; i<NO_SAMPLES; i++) {                         
        v = Buffer[i+offset2];                              
        AccMS64 +=  (uint64)(v*v) * Window[i];              
    }

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Uwe Bonnes
Chief

I fear you have to understand both ways DMA is implemented anf you have to rewrite DMA setup and runtime code.