How to solve the stm32g4 internal RTC module drift problem (15 seconds in 2 days)?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-24 1:20 PM
I am using the stm32g474rct6 RTC module. over a duration of 2 days, the drift was over 15 seconds. I tested it in standard room conditions. How can I solve this problem ?
- Labels:
-
RTC
-
STM32G4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-24 2:32 PM
86ppm, it's not THAT bad.
First, if you are Cube, make sure this is not consequence of the unnecessary initialization (that would delay the clock half a second in average per reset).
Slow/fast running oscillator can be compensated digitally within RTC, read RTC smooth digital calibration subchapter in RM; but maybe you should tweak the load capacitors first to get closer to nominal. Read AN2867.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-25 1:50 AM
Thanks for answer.
I use it as shown in the picture below. Is there any problem for this structure ? I guess the block I marked creates a delay every time I run the main function, is it right ?
thanks in advance.
int main(void)
{
.....
o_RTC_Init();
....
}
/**
* @brief provide to initialize the RTC module once reading HAL_RTCEx_BKUPRead.
*/
uint8_t o_RTC_Init(void)
{
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_12;
hrtc.Init.AsynchPrediv = 127;
hrtc.Init.SynchPrediv = 255;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if(HAL_RTC_Init(&hrtc) != HAL_OK){
return FALSE;
}
if(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR0) != 0x32F2){
/* RTC configuration */
s_time.Hours = 1;
s_time.Minutes = 0;
s_time.Seconds = 0;
s_time.TimeFormat = RTC_HOURFORMAT12_AM;
s_time.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
s_time.StoreOperation = RTC_STOREOPERATION_RESET;
s_date.Year = 20;
s_date.Month = RTC_MONTH_JANUARY;
s_date.Date = 1;
s_date.WeekDay = RTC_WEEKDAY_WEDNESDAY;
if(HAL_RTC_SetDate(&hrtc, &s_date, RTC_FORMAT_BIN) != HAL_OK){
return FALSE;
}
if(HAL_RTC_SetTime(&hrtc, &s_time, RTC_FORMAT_BIN) != HAL_OK){
return FALSE;
}
HAL_RTCEx_BKUPWrite(&hrtc, RTC_BKP_DR0, 0x32F2);
}else{
/* Clear source Reset Flag */
__HAL_RCC_CLEAR_RESET_FLAGS();
}
v_RTC_CheckDateTime();
return TRUE;
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-25 2:17 AM