cancel
Showing results for 
Search instead for 
Did you mean: 

How to select gain in STM32H743 ADC

NVerm.2
Associate II

How to select gain in STM32H743 ADC? I looked up all the configurations/parameters but don't see how can I amplify (select gain) for input channel? I want to measure current which is mV signal.

1 ACCEPTED SOLUTION

Accepted Solutions

Correct, there is no built-in amplifier.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @NVerm.2​, to the community!

If you want to measure something in the millivolt range, you have to connect an amplifier stage in front of the ADC input. 

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Peter,

Yes, thanks, it means it does not have amplifier built-in where I can select gain x.

Correct, there is no built-in amplifier.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.