2023-11-30 5:56 AM
Hello,
I have a program that works in DMA but I would like to put a function to know when the transfer in the DMA is finished so that I can recover the data continuously. Do you have any information on this ? Here is part of my code
HAL_SAI_RegisterCallback(&hsai_BlockA1, HAL_SAI_RX_HALFCOMPLETE_CB_ID, HAL_SAI_RxHalfCpltCallback);
HAL_SAI_RegisterCallback(&hsai_BlockA1, HAL_SAI_RX_COMPLETE_CB_ID, HAL_SAI_RxCpltCallback);
fresult= HAL_SAI_Init(&hsai_BlockA1);
if (fresult != HAL_OK)
{
return HAL_ERROR;
}
HAL_SAI_RegisterCallback(&hsai_BlockB1, HAL_SAI_TX_HALFCOMPLETE_CB_ID, HAL_SAI_TxHalfCpltCallback);
HAL_SAI_RegisterCallback(&hsai_BlockB1, HAL_SAI_TX_COMPLETE_CB_ID, HAL_SAI_TxCpltCallback);
fresult= HAL_SAI_Init(&hsai_BlockB1);
if (fresult != HAL_OK)
{
return HAL_ERROR;
}
fresult = HAL_SAI_Receive_DMA(&hsai_BlockA1, (uint8_t *)playbuf_RX, (sizeof(playbuf_RX))/4);
if (fresult != HAL_OK)
{
return HAL_ERROR;
}
fresult = HAL_SAI_Transmit_DMA(&hsai_BlockB1, (uint8_t *)playbuf , (sizeof(playbuf))/4);
if (fresult != HAL_OK)
{
return HAL_ERROR;
}
Thanks in advance
Solved! Go to Solution.
2023-11-30 12:48 PM
Another entitled brat. Thanks, Generation Arduino!
2023-11-30 1:23 PM
@David Littell wrote:Another entitled brat. Thanks, Generation Arduino!
We talk about everything except the subject. You deserve to be the KING my friend ! Not the Senior III.