2018-12-04 11:10 PM
Hello,
I try to run an ISR (void TIM3_IRQHandler(void)) in the ITCM RAM area.
I'm new with scatter-files. Anybody has an example?
(NUCLEO-H743ZI, Keil uVision)
Regards
Jakob
Solved! Go to Solution.
2018-12-05 4:06 AM
2018-12-05 4:06 AM
Check out AN4296 at https://www.st.com/resource/en/application_note/dm00083249.pdf
2018-12-05 4:50 AM
Thank you
2018-12-05 5:39 AM
One could call out the stm32h7xx_it.o (the object) in the scatter file and direct it into a RAM Region
Real problem is everything you might call, or library code.
2018-12-06 7:03 AM
Thank you for your help. First test was succesful.
Regards
2019-06-11 1:17 AM
With help of the AppNote I put the HAL lib and the FreeRTOS files (*.o) successful to the ITCM RAM region (gcc). But if I add the *_it.o file like in the example it will rise hardfault ISR after a while (interestingly successful). What could be the reason for this? Some interrupts seems to work without problem...