cancel
Showing results for 
Search instead for 
Did you mean: 

How to increase GPIO on any STM32 MCU?

parth kothiya
Senior

I want to design PLC using STM32 MCU so for that I need to extend its GPIO pins how can i do this?

Adding another MCU or shift registers any other ideas?

Main cpu having MCU and another io modules added is communicate with ​main cpu using protocol like SPI , I2C ..

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Pavel A.
Super User

Use GPIO expanders on I2C or SPI.

Javier1
Principal

How fast and how many GPIOS do you need.

Shift registers are the fastest and cheapest of them all.(careful with the transients)

They need 3 GPIOS to be driven (clock, latch ,data) and you could daisy chain them.

I would use the SPI/i2c options only if i was already using the spi/i2c and i culdnt spare gpios to drive the shift registers

Available for consulting/freelancing , hit me up in https://github.com/javiBajoCero
Muhammed Güler
Senior III

Additional ICs on a single card often cost more than a larger model of the same processor. For additional modules, you can use a circuit with an SPI/I2C IO expander IC, or you can design a circuit that can be configured for different features with a MCU.

I would like to remind you that it is more difficult to debug designs with multiple MCUs.