2024-11-22 02:46 AM
I have two STM32F407IGT6 chips, and I need help understanding the markings printed on their surfaces.
I would like to know:
Any detailed guidance or resources to decode this information would be greatly appreciated. Thank you!
Solved! Go to Solution.
2024-11-24 07:18 PM
VQ if a diffusion plant in France for the wafer
AA29x is a production/packaging plant in Taiwan
You can determine the chip stepping via the DBGMCU / DEV_ID, and associate that with an Errata
The production date might shed some light on the options enabled on the F4 dies, ie Ethernet,Crypt, etc
2024-11-22 06:45 AM - edited 2024-11-22 06:50 AM
Hello,
The information needed by the user is provided in the datasheet:
We don't provide detailed explanation. And the two chips are genuine.
Many new chips have 2D QR code marking. for more details you can contact your local FAE/Sales.
2024-11-24 06:27 PM
Hello,
Thank you for the response. I have already reviewed the datasheet and understand how to read the date/time information printed on the chips.
However, I have a specific question regarding the markings:
What do these specific codes represent?
The reason I am asking is that I am using both chips in the same circuit and with identical code, but I am observing a difference in the Ethernet functionality:
Could you please explain why there is this difference? Are the markings related to internal revisions or production variations that affect Ethernet compatibility?
Thank you for your assistance!
2024-11-24 07:18 PM
VQ if a diffusion plant in France for the wafer
AA29x is a production/packaging plant in Taiwan
You can determine the chip stepping via the DBGMCU / DEV_ID, and associate that with an Errata
The production date might shed some light on the options enabled on the F4 dies, ie Ethernet,Crypt, etc
2024-11-25 05:42 PM
Thank you for the clarification. I understand now, and I appreciate your help!