cancel
Showing results for 
Search instead for 
Did you mean: 

How to identify information printed on STM32F407IGT6 chips?

Muk
Associate II

I have two STM32F407IGT6 chips, and I need help understanding the markings printed on their surfaces.

  • Images attached:
    • First chip: "STM32F407IGT6 AA295 VQ 6 TWN AA 342"
    • Second chip: "STM32F407IGT6 VQ249473 AA297 TWN AA 318"

I would like to know:

  1. What each line of the markings represents?
  2. How to verify the authenticity of these chips?
  3. If there are any important differences between these two chips based on the markings?

Any detailed guidance or resources to decode this information would be greatly appreciated. Thank you!

Muk_0-1732272258299.png

Muk_1-1732272261127.png

 

1 ACCEPTED SOLUTION

Accepted Solutions

VQ if a diffusion plant in France for the wafer

AA29x is a production/packaging plant in Taiwan

You can determine the chip stepping via the DBGMCU / DEV_ID, and associate that with an Errata

https://www.st.com/resource/en/reference_manual/rm0090-stm32f405415-stm32f407417-stm32f427437-and-stm32f429439-advanced-armbased-32bit-mcus-stmicroelectronics.pdf#page=1716

The production date might shed some light on the options enabled on the F4 dies, ie Ethernet,Crypt, etc

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

4 REPLIES 4
SofLit
ST Employee

Hello,

The information needed by the user is provided in the datasheet:

SofLit_0-1732286374880.png

We don't provide detailed explanation. And the two chips are genuine.

Many new chips have 2D QR code marking. for more details you can contact your local FAE/Sales.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.
Muk
Associate II

Hello,

Thank you for the response. I have already reviewed the datasheet and understand how to read the date/time information printed on the chips.

However, I have a specific question regarding the markings:

  • AA295 VQ 6 on one chip.
  • VQ249473 AA297 on the other chip.

What do these specific codes represent?

The reason I am asking is that I am using both chips in the same circuit and with identical code, but I am observing a difference in the Ethernet functionality:

  • The chip marked AA297 VQ b works with both newer and older switches.
  • The chip marked VQ249473 AA297 only works with newer switches.

Could you please explain why there is this difference? Are the markings related to internal revisions or production variations that affect Ethernet compatibility?

Thank you for your assistance!

VQ if a diffusion plant in France for the wafer

AA29x is a production/packaging plant in Taiwan

You can determine the chip stepping via the DBGMCU / DEV_ID, and associate that with an Errata

https://www.st.com/resource/en/reference_manual/rm0090-stm32f405415-stm32f407417-stm32f427437-and-stm32f429439-advanced-armbased-32bit-mcus-stmicroelectronics.pdf#page=1716

The production date might shed some light on the options enabled on the F4 dies, ie Ethernet,Crypt, etc

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you for the clarification. I understand now, and I appreciate your help!