cancel
Showing results for 
Search instead for 
Did you mean: 

how to give program to L031K6 when detached from board?

DU2
Associate II

hello, I am using L031K6 with UM1956 board.

I am trying ultra low power sensor project with it.

I would like to detach the board(UM1956) then make own circuit

in that case, how to give program to L031K6?

3 REPLIES 3

Presumably you'd need to wire back up the SWDIO/SWCLK connections, or use one of the methods provided by the system boot loader (see app note AN2606)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

thanks for answer. but when I wired up that connections and give program to L031K6 by JLINK 4 pin,

what option should I set in IAR compiler? I am using IAR Imbedded workbench IDE (EWARM 7.0) ​ with dongle.

Make sure that you are providing VDD and VDDA to MCU. what error massage does IAR show?