2020-07-30 09:38 PM
hello, I am using L031K6 with UM1956 board.
I am trying ultra low power sensor project with it.
I would like to detach the board(UM1956) then make own circuit
in that case, how to give program to L031K6?
2020-07-30 09:53 PM
Presumably you'd need to wire back up the SWDIO/SWCLK connections, or use one of the methods provided by the system boot loader (see app note AN2606)
2020-07-30 10:47 PM
thanks for answer. but when I wired up that connections and give program to L031K6 by JLINK 4 pin,
what option should I set in IAR compiler? I am using IAR Imbedded workbench IDE (EWARM 7.0) with dongle.
2020-07-30 11:43 PM
Make sure that you are providing VDD and VDDA to MCU. what error massage does IAR show?