2022-01-31 3:31 AM
Hi!!
I am using a STM32F4 Discovery board. I am using the ADC1 and ADC2, both with DMA. I need the conditional to know which ADC was the one that finished reading data. I tried if(hadc->Instance == ADC1) but it only works when DMA is not used.
Could you help me to get the identifier of the ADC when using DMA?
2022-01-31 9:00 AM
2022-01-31 9:09 AM
The problem is in HAL_ADC_MspInit(): HAL DMA handle for ADC2 is not configured
in "else if(hadc->Instance==ADC2)", there should be:
/* ADC2 DMA Init */
/* ADC2 Init */
hdma_adc2.Instance = DMA2_Stream2;
hdma_adc2.Init.Channel = DMA_CHANNEL_1;
hdma_adc2.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_adc2.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_adc2.Init.MemInc = DMA_MINC_ENABLE;
hdma_adc2.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
hdma_adc2.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
hdma_adc2.Init.Mode = DMA_CIRCULAR;
hdma_adc2.Init.Priority = DMA_PRIORITY_MEDIUM;
hdma_adc2.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_adc2) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hadc,DMA_Handle,hdma_adc2);with hdma_adc2 declared in the same way as hdma_adc1 (global variable).
If you started from CubeMX, then something is missing in the GUI configuration.
Best regards
Philippe
2022-01-31 9:27 AM
I understand, the ADC2 wasn't configured with DMA because I wasn't using it. Remove the ADC 2 configuration from the GUI.
My question now is, how should I build the conditional? because
if(hadc->Instance == ADC1) doesn't work, I'm doing it wrong and it's not clear to me why.
Thank you very much for your time!
2022-01-31 9:29 AM
It worked!!! I had to set it up like this:
if (hadc->DMA_Handle->Instance == DMA2_Stream0){
Thank you very much to all!!