2025-12-17 7:22 AM - last edited on 2025-12-19 1:40 AM by mƎALLEm
I'm trying to receive some data over CAN (using Kvaser CanKing 500 kbit/s) and display it on a Riverdi 12.1" display. In fdcan.c, I have:
void MX_FDCAN1_Init(void)
{
/* USER CODE BEGIN FDCAN1_Init 0 */
FDCAN_FilterTypeDef sFilterConfig; // the required filter ID can be found in the struct
/* USER CODE END FDCAN1_Init 0 */
/* USER CODE BEGIN FDCAN1_Init 1 */
/* USER CODE END FDCAN1_Init 1 */
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL; // FDCAN_MODE_INTERNAL_LOOPBACK; // FDCAN_MODE_NORMAL;
hfdcan1.Init.AutoRetransmission = DISABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = DISABLE;
hfdcan1.Init.NominalPrescaler = 1;
hfdcan1.Init.NominalSyncJumpWidth = 32;
hfdcan1.Init.NominalTimeSeg1 = 127;
hfdcan1.Init.NominalTimeSeg2 = 32;
hfdcan1.Init.DataPrescaler = 1;
hfdcan1.Init.DataSyncJumpWidth = 10;
hfdcan1.Init.DataTimeSeg1 = 29;
hfdcan1.Init.DataTimeSeg2 = 10;
hfdcan1.Init.MessageRAMOffset = 0;
hfdcan1.Init.StdFiltersNbr = 1;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.RxFifo0ElmtsNbr = 32;
hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_64;
hfdcan1.Init.RxFifo1ElmtsNbr = 0;
hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
hfdcan1.Init.RxBuffersNbr = 1;
hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8;
hfdcan1.Init.TxEventsNbr = 0;
hfdcan1.Init.TxBuffersNbr = 1;
hfdcan1.Init.TxFifoQueueElmtsNbr = 1;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
HAL_GPIO_TogglePin(USR_LED_1_GPIO_Port, USR_LED_1_Pin);
/* USER CODE BEGIN FDCAN1_Init 2 */
FDCAN_FilterTypeDef sFilter = {0};
// Route standard ID 0x123 to FIFO0
sFilter.IdType = FDCAN_STANDARD_ID;
sFilter.FilterIndex = 0;
sFilter.FilterType = FDCAN_FILTER_MASK;
sFilter.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilter.FilterID1 = 0x111; // ID
sFilter.FilterID2 = 0x000; // mask: all bits must match
if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilter) != HAL_OK)
{
Error_Handler();
}
HAL_FDCAN_ConfigGlobalFilter(
&hfdcan1,
FDCAN_ACCEPT_IN_RX_FIFO0, // Non-matching standard IDs
FDCAN_ACCEPT_IN_RX_FIFO0, // Non-matching extended IDs
FDCAN_REJECT_REMOTE, // Standard remote
FDCAN_REJECT_REMOTE // Extended remote
);
if (HAL_FDCAN_Start(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0);
FDCAN_TxHeaderTypeDef txh = {0};
uint8_t txd[8] = {0};
txh.Identifier = 0x123;
txh.IdType = FDCAN_STANDARD_ID;
txh.TxFrameType = FDCAN_DATA_FRAME;
txh.DataLength = FDCAN_DLC_BYTES_8;
txh.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
txh.BitRateSwitch = FDCAN_BRS_OFF;
txh.FDFormat = FDCAN_CLASSIC_CAN;
txh.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
txh.MessageMarker = 0;
uint32_t value = 424242; // whatever you want to see
txd[0] = (uint8_t)(value);
txd[1] = (uint8_t)(value >> 8);
txd[2] = (uint8_t)(value >> 16);
txd[3] = (uint8_t)(value >> 24);
//rest bytes can be 0
HAL_FDCAN_ActivateNotification(&hfdcan1,
FDCAN_IT_TX_COMPLETE | FDCAN_IT_BUS_OFF | FDCAN_IT_ERROR_PASSIVE | FDCAN_IT_ERROR_WARNING,
0);
if (HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &txh, txd) != HAL_OK)
{
Error_Handler();
}
/* USER CODE END FDCAN1_Init 2 */
}
If I use FDCAN_INTERNAL_LOOPBACK, I can see "424242" as expected on the display. But in FDCAN_MODE_NORMAL, I cannot send anything. On CanKing, I simply see an error frame received from the display. Is there any documentation or sample code I can refer to, to make this work? IF needed, I can share the Git repo for the project.
Also, is it possible to debug the code from the CubeIDE?
Solved! Go to Solution.
2025-12-19 1:38 AM - edited 2025-12-19 4:08 AM
Hello,
You didn't show the clock configuration.
Did you select HSE with an external crystal as clock source for FDCAN? You need to use HSE with an external crystal.
Check also the wiring.
2025-12-19 1:38 AM - edited 2025-12-19 4:08 AM
Hello,
You didn't show the clock configuration.
Did you select HSE with an external crystal as clock source for FDCAN? You need to use HSE with an external crystal.
Check also the wiring.