cancel
Showing results for 
Search instead for 
Did you mean: 

Give me a second example on embedded programming on my Nucleo board

Adev.1
Associate III

Hi all,

I've installed STM32CubeIDE, STM32CubeMX plus STM32CubeProgrammer. As well as, I've written a simple C++ project to blink the LED of my STM32NucleoF411RE board when it's connected to my Windows machine, as my first embedded programming project. Moreover, I'm able to write a typical piece of code in C++ to output a result, just like console applications, and observe that output on the IDE too. I've done these based on self-education and must make progress this way yet.

What do you suggest that I work on as the second project/example/exercise to be a little more advanced than what I did via my board, please?

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
KnarfB
Super User

There are so many choices...

  • connect a cheap sensor breakout board via I2C or SPI bus and read-out measurements
  • use ADC channels to measure analog voltages like from a photo resistor
  • connect a tiny OLED display via SPI bus
  • generate PWM signals to control a servo motor, or a buzzer/speaker
  • ...

You might get some ideas by browsing board vendor sites like Adafruit, Sparkfun, ...

hth

KnarfB

TDK
Super User

Get the ST-Link VCP working.

If you feel a post has answered your question, please click "Accept as Solution".
Adev.1
Associate III

Thank you for your answers.

Let me please before all else tell you of all the embedded stuff I have at hand for embedded programming:

  • Nucleo STM32 F411RE board
  • Breadboard
  • A blue pill board (stm32f103c8)
  • a bunch of wires

Now please tell me which of the projects above is the simplest one which can be done using the embedded stuff above?

That will be my second embedded programming ever, after blink LED project.