How to generate two PWM with 180Deg phase shift with STM32F30303 advance timer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-05-14 1:26 AM
Hello All,
I am very new to STM32F303 device. I want to generate two PWM from Advance timer TIM1 or TIM8, with same frequency, Same duty cycle but 180deg phase shift. Can any one help me out to configure the timer or help me out how i can generate the same as required. I will appreciate your replies.RegardsMukesh #stm32f303 #phase-shifted-pwm- Labels:
-
STM32F3 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-05-14 2:07 AM
There are perhaps a couple of ways of doing this. Given they share a common synchronous clock source you can develop/control a phase relationship via the TIMx->CNT registers. If the frequency isn't too high you could also use the Update interrupt to alternate the firing of each, which would permit the signal to be generated by two channels of the same timer.
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
‎2013-05-14 3:59 AM
Don't TIM1 and TIM8 offer complementary outputs already.
Section16.3.14 in the Reference Manual D02258 Rev 2:
''The advanced-control timers (TIM1/TIM8) can output two complementary signals andmanage the switching-off and the switching-on instants of the outputs. ''
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-05-14 8:08 AM
I'm not sure that complementary and 180-degree phase shift mean the same thing.
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
‎2013-05-15 11:24 PM
I'm investigating something similar.
I wanted two signals 180 degrees apart with deadtime AND individually controllable dutycycles. Just using the complementary outputs would solve the first part but you can't control the duty cycles individually using the complementary signal. The solution I came up with for my project is using TIM1_CH1 and TIM2_CH2 and as long as we don't use longer duty cycles than 50% we're golden. But we've lost some of the safety functions from using the complemntary outputs :( I'm still not completely convinced it isn't doable with the complimentary outputs...) The way I set it up is i set the counter mode to Center-aligned mode 3 (CMS[1:0]=11 in TIM1_CR1). And then use PWM mode 1 for TIM1_CH1 (OC1M = 0110 in TIM1_CCMR1) and PWM mode 2 for TIM1_CH2 (OC2M = 0111). Now they'll share the same frequency and if you use the same pulse length in TIM1_CCR1 and TIM1_CCR2 they´ll have the same duty cycle as well. Here's some copy paste: TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_CenterAligned3; TIM_TimeBaseStructure.TIM_Period = TimerPeriod; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable; TIM_OCInitStructure.TIM_Pulse = Channel1Pulse; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_Low; TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Reset; TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCIdleState_Reset; TIM_OC1Init(TIM1, &TIM_OCInitStructure); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2; TIM_OCInitStructure.TIM_Pulse = Channel2Pulse; TIM_OC2Init(TIM1, &TIM_OCInitStructure);