2020-09-11 10:17 PM
I have connected a sine wave of amplitude 3V with 1.5V shifted above the zero to 12-bit ADC channel by using dsPIC33FJ32MC204 controller and stored in an array. I want to detect the max value out of five samples because after the five samples my data is repeating, so please give me any suggestion on it. I am getting output as a zero.
Solved! Go to Solution.
2020-09-14 06:17 AM
If(I<arrayLenght)
{
} This case is to fill the array with adc values
When array will be filled completely then
If(I==arrayLength)
{
} This section will find the max value
Because until the array is not completed no need to check for max value
The code you want to write will never fill the array completely because
Each time i will be 0
You have take another variable for the loop to do by your way
array[i] =adc_value;
for(j=0;j<8;j++)
{
if(array[j] > max)
{
max = array[j];
}
sprintf(data1,"%.2f",max);
LCD_String_xy(1,1,data1);
max=0;
}
i++;
if(i == 😎
{
i = 0;
}
This will work
2020-09-12 02:34 AM
#define arrayLength 5
unsigned int array[arrayLength]; //Array values should be updated with ADC values.
unsigned int i, max = 0;
void main()
{
for(i=0;i<sizeof(array)/sizeof(array[0]);i++)
{
if(array[i] > max)
{
max = array[i];
}
}
//here after the loop completion you can get the maximum value in variable max
}
You can find max number in a array by this way.
2020-09-13 09:07 PM
@sanju Thanks for your quick response sir and your logic is working properly and getting max value accurately but facing one problem that as data is real time ,so how can i take infinite data in array means how can i update array values with ADC values?
Thanks in advance.
2020-09-13 11:14 PM
First of all, you can't store infinite data in array because RAM size of your device is 2 KB. so you have to define arrayLength
#define arrayLength 5(you have to set it first).
suppose you have this define it as 8
then code like this
#define arrayLength 8
unsigned int array[arrayLength]; //Array values should be updated with ADC values.
unsigned int i=0, max = 0;
void main()
{
while(1)
{
if(i<arrayLength )
{
//Read adc value and assign in array
array[i] = adc_value;
i++;
}
if(i == arrayLength )
{
for(i=0;i<sizeof(array)/sizeof(array[0]);i++)
{
if(array[i] > max)
{
max = array[i];
}
}
//here after the loop completion you can get the maximum value in variable max
i=0;
//Read adc value and assign in array
array[i] = adc_value;
i++;
}
// do your other tasks here
//Put some delay if required between adc samples.
}
}
2020-09-14 05:42 AM
@sanju Thanks for your reply sir. I have to detect max value in both cases (i<arrayLength & i == arrayLength ),but in one condition i.e i<arrayLength max value detection is missing. And another thing is can i replace the whole code by writing the code like-
array[i] =adc_value;
for(i=0;i<8;i++)
{
if(array[i] > max)
{
max = array[i];
}
sprintf(data1,"%.2f",max);
LCD_String_xy(1,1,data1);
max=0;
}
if(i == 😎
{
i = 0;
}
}
2020-09-14 06:17 AM
If(I<arrayLenght)
{
} This case is to fill the array with adc values
When array will be filled completely then
If(I==arrayLength)
{
} This section will find the max value
Because until the array is not completed no need to check for max value
The code you want to write will never fill the array completely because
Each time i will be 0
You have take another variable for the loop to do by your way
array[i] =adc_value;
for(j=0;j<8;j++)
{
if(array[j] > max)
{
max = array[j];
}
sprintf(data1,"%.2f",max);
LCD_String_xy(1,1,data1);
max=0;
}
i++;
if(i == 😎
{
i = 0;
}
This will work
2020-09-14 06:50 AM
@sanju I got your point sir but once j becomes greater than 8,it will never goes in for loop and my data is real time data, so I have to do it continuously. I think instead of i = 0, it should be j = 0 ?
2020-09-14 08:16 PM
Dear Mohan,
j is running a loop
i.e. for(j=0;j<8;j++)
so if j>8, your code is in while loop, so every time j will be initialized with j=0 to start the loop.
i and j are separately working i is filling array and j is finding max value by running a loop
2020-09-14 10:41 PM
@sanju Now everything is cleared sir, thank you and special thanks to your patience for clearing my basic doubts.