how to convert CAN loopback example code to CAN normal mode?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-28 4:34 AM
I am using CAN loopback example code for my STM23l476RG evaluation board (with new API's) and it is working fine, but how port same example to normal mode I am not getting please help.
- Labels:
-
CAN
-
STM32L4 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-28 6:58 AM
Look for Network examples. You need two nodes for Normal mode to be functional, as a receiving node needs to acknowledge the packets.
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
‎2018-10-29 2:56 AM
I am using network example with two evaluation board along with MCP2551 CAN tranceiver. One board I configured as tx and another as rx, but I am not able to receive the data in Rxdata buffer
suggest me something.
//this is my TX part code
CanHandle.Init.TimeTriggeredMode = DISABLE;
CanHandle.Init.AutoBusOff = DISABLE;
CanHandle.Init.AutoWakeUp = DISABLE;
CanHandle.Init.AutoRetransmission = ENABLE;
CanHandle.Init.ReceiveFifoLocked = DISABLE;
CanHandle.Init.TransmitFifoPriority = DISABLE;
CanHandle.Init.Mode = CAN_MODE_NORMAL;
CanHandle.Init.SyncJumpWidth = CAN_SJW_1TQ;
CanHandle.Init.TimeSeg1 = CAN_BS1_6TQ;
CanHandle.Init.TimeSeg2 = CAN_BS2_2TQ;
CanHandle.Init.Prescaler = 5;
if(HAL_CAN_Init(&CanHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/*##-3- Start the CAN peripheral ###########################################*/
if (HAL_CAN_Start(&CanHandle) != HAL_OK)
{
/* Start Error */
Error_Handler();
}
/*##-4- Start the Transmission process #####################################*/
TxHeader.StdId = 0x11;
TxHeader.RTR = CAN_RTR_DATA;
TxHeader.IDE = CAN_ID_STD;
TxHeader.DLC = 2;
TxHeader.TransmitGlobalTime = DISABLE;
TxData[0] = '$';
TxData[1] = '#';
/* Request transmission */
if(HAL_CAN_AddTxMessage(&CanHandle, &TxHeader, TxData, &TxMailbox) != HAL_OK)
{
/* Transmission request Error */
Error_Handler();
}
//this is RX side code
configuring filter and receiving msg
sFilterConfig.FilterBank = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = 0x11 << 5;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0xFFFF;
sFilterConfig.FilterMaskIdLow = 0xFFFF;
sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.SlaveStartFilterBank = 14;
if(HAL_CAN_ConfigFilter(&CanHandle, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}
/* Get RX message */
if (HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
{
/* Reception Error */
Error_Handler();
}
/* Display LEDx */
if ((RxHeader.StdId == 0x11) && (RxHeader.IDE == CAN_ID_STD) && (RxHeader.DLC == 2))
{
// code for LED
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-29 3:28 AM
Don't the EVAL series boards​ have CAN ports and transceivers already?
What board specifically do you have? A DISCO or NUCLEO? ​
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
‎2018-10-29 3:36 AM
No CAN transceiver. It is NUCLEO. MCP2551 CAN tranceiver I am using.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-25 10:32 PM
Do you get the answer? I am facing same problem.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-26 7:01 AM
If it works with loopback, it should work with two boards with the same SW and CAN lines connected, without loopback.