2021-10-18 10:41 PM
If I vary any one channel Input through POT, it is reflecting in another ADC Channel also... can anyone help me regarding this ?
2021-10-19 9:38 PM
Sure Thanks for the Suggestion..
along with this i will try to use configurations with another channels too
Will update you , Incase If I need any help regarding this, Thanks again @Georgy Moshkin
2021-10-20 10:39 AM
Is There any function to disable Specific ADC Channel after Analog to Digital Conversion
@Georgy Moshkin
2021-10-20 6:54 PM
Most straight forward way is de-initializing/stopping peripheral using functions like HAL_ADC_DeInit(), and then initializing/starting again with new parameters. Some things may be performed without de-initialization, bust must dig into reference manual to find out, some hints may be found in HAL source code comments (stm32..._hal_adc.c).
2021-10-21 5:21 AM
Should I select another controller which is Having Two ADC's(ADC1,ADC2) and CAN Protocol, If you know any controller having this features suggest me ?
@Georgy Moshkin
2021-10-21 6:43 AM
Probably no, there are a lot of channels, select channels and make sure those pins are not used on your Nucleo board for something else, or remove solder bridges according to Nucleo documentation