cancel
Showing results for 
Search instead for 
Did you mean: 

How to chose a pin compatible processor with larger RAM - STM32F756ZGT6 144-pin

AHuss.9
Associate II

Dear all,

Apologies if this is a naïve post.

I am trying to find a processor for the product that I am working on with larger RAM and FLASH but it must remain pin compatible to minimise code changes. The current processor is this "STM32F756ZGT6". With the current application its RAM is throttling at 100% and more features are still pending to be added. Therefore, if I can find another processor with the same pinout then the problem will be resolved.

Any help would be appreciated please? 

Many thanks

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION
6 REPLIES 6
AScha.3
Super User

Hi,

if you click pinout in Cube , then can select : list pin compatible... try:

AScha3_0-1716486228810.png

 

+

just guessing : stm32H743ZI (most pins compatible) , 1MB ram, 2MB flash.

If you feel a post has answered your question, please click "Accept as Solution".
AHuss.9
Associate II

Dear AScha,

In my case it only gives me one processor. Many thanks for your reply though.

AHuss9_0-1716486700507.png

 

What other Series did you check box?

The 144-pin devices have the broadest pin compatibility, unless you are using a function/peripheral that doesn't map exactly.

For that F7 die I don't think there's a more RAM/FLASH option within the family.

I'd expect there's an H743 which would fit

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
AHuss.9
Associate II

Dear Tesla Delorean,

I was trying some others and found this one which seems to have the same pinout but 2M Flash and 512KB RAM.
Is this a good swap do you think?

https://www.st.com/en/microcontrollers-microprocessors/stm32f765zi.html#sample-buy

 

Dear AScha,

You have provided an excellent suggestion. I will look into this further. 1M RAM is absolutely charming,
Many thanks Sir.