cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-67W61M1 + NUCLEO-F44 compatibility

Youssef Harby
Associate

Dear ST Support Team,
I would like to ask about the compatibility of using the X-NUCLEO-67W1M1 expansion board based on ST67W611M1 with the NUCLEO-F446RE development board.
I had read the **X-CUBE-ST67W61 Data brief document on page 3**  

"The X-CUBE-ST67W61 Expansion Package runs on STM32 32-bit microcontrollers based on
• The Arm® Cortex®‑M33 and Cortex®‑M55 processors with Arm® TrustZone®
• The Arm® Cortex®‑M7 processor"

So, my questions are:

1. Is the X-NUCLEO-67W61M1 hardware compatible with NUCLEO-F44 (Cortex M4 processor)? 
2. Can I use raw SPI + AT commands without X-CUBE-ST67W61?, Has anyone done this on F44(Cortex M4 processor)? 

3. Any known working example or GitHub project for (Cortex M4 processor)+ X-NUCLEO-67W61M1?

1 ACCEPTED SOLUTION

Accepted Solutions
Issamos
Lead III

Hello @Youssef Harby 

 

  • The X-NUCLEO-ST67W61M1 and the X-CUBE-ST67W61 are both compatible with the STM32F4 series (including the MCU embedded on the NUCLEO-F446RE). 
  • For The configuration of the WIFI module with or without the X cube package. I suggest you to have a look at the WIKI pages available here that will give you all what you need for all applications you want to make.
  • For the examples, they are not available for the STM32F4 series but you can use those made for the STM32U5, STM32H5, STM32N6 and STM32H7RS as a reference and with the content of The wikis you will be able to make your own applications.

Best Regards.

II

View solution in original post

2 REPLIES 2
Issamos
Lead III

Hello @Youssef Harby 

 

  • The X-NUCLEO-ST67W61M1 and the X-CUBE-ST67W61 are both compatible with the STM32F4 series (including the MCU embedded on the NUCLEO-F446RE). 
  • For The configuration of the WIFI module with or without the X cube package. I suggest you to have a look at the WIKI pages available here that will give you all what you need for all applications you want to make.
  • For the examples, they are not available for the STM32F4 series but you can use those made for the STM32U5, STM32H5, STM32N6 and STM32H7RS as a reference and with the content of The wikis you will be able to make your own applications.

Best Regards.

II

Hello @Issamos

Thank you for the guidance.

I reviewed the ST Wiki pages you linked and followed the steps to configure the CLI application example for the X-NUCLEO-ST67W61M1 on the NUCLEO-F446RE (STM32F4 series). The project builds successfully.

However, when running the generated code directly on the F446RE, it triggers a Hard Fault immediately after start. Interestingly, when I debug the same binary using STM32CubeIDE / ST-LINK, the application executes correctly without any fault. Is that maybe because of the legacy FreeRTOS of the STM32F4?!

Best regards,

Harby