2021-05-28 1:24 AM
Hai,
I am working on the stm32f070c6 MCU , I just want to enable the multiple channels of ADC using polling method, all the channels are enabled for suppose when I connect the sensor to the AD0 pin the values coming from the sensor effects the all the channels(which I don't use(kept as floating) ), when I connect the all the channels to the 3.3V it is exact values at all the channels but when I use 1 or 2 channels the other channels are also effected and gives the values , actually I put a min value as 100 , if it greater than 100mv at particular channel it transmit the adc value, if it is less than 100mv it doesn't transmit the adc values to the serial monitor , problem is when i use less than 8 channels (either 1 or 2) the values are incorrect and effects to the all other channels , how can I overcome this problem if any one have idea please give a suggestion
Thanks and Regards
RAJ
2021-05-28 1:51 AM
All channels of one ADC use the Sample&Hold capacitor.
This forms a simple first-order RC element, which needs to be charged / discharged to the input voltage of the channel.
If your sample times are too short, you get this bleed-over effect.
Calculate the RC behavior according to the STM datasheet and your input schematics, and adapt the required sample time accordingly.