2018-11-28 8:54 AM
Hi,
I am developing a motor control application for a servo that is controlled in impulses. So, in my case, the number of impulses represents the number of steps.
For that, I am using the TIM1 in PWM mode using One-Pulse. To account for the number of steps/impulses I use the RCR. To change the RCR val I set the corresponding bit of EGR to generate an update of the TIM1 registers.
The problem arises when I want to generate a small PWM period (4 us in the figure above) I have created a small trial application to test the functionality of my approach. So, I am generating 3 sequences of impulses using 3 different values (0, 1 and 2) for RCR. Because the RCR val corresponds to RCR+1 pulses, the result has to be 6 impulses, which is achieved. However this result is not good because when the RCR value is updated, a delay is introduced. See the picture below.
To accomplish this task I used interrupts for update events, namely:
The hardware is a prototype board designed around the microcontroller STM32F103C8T. Other things important to mention:
__HAL_TIM_ENABLE_IT(&htim1, TIM_IT_UPDATE);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
Finally, I somehow would like to update the RCR and TIM1 registers without treat the first update interrupt from above. I belive, there I lose time...
Thank you for your attention and I look forward for some advises. Se the code from interrupt service routine below:
/**
* @brief This function handles TIM1 update interrupt.
*/
void TIM1_UP_IRQHandler(void)
{
/* USER CODE BEGIN TIM1_UP_IRQn 0 */
/* USER CODE END TIM1_UP_IRQn 0 */
// I commented the line below because I do not want to evaluate all the possible events that generated this interrupt. In my case it is clear that only the update event
// will generate interrupts
//HAL_TIM_IRQHandler(&htim1);
__HAL_TIM_CLEAR_IT(&htim1, TIM_IT_UPDATE);
if(flag_update_event)
{
// Make this flag FLASE, because next time this interrupt will be enterred, will be because the RCR value overflowed
flag_update_event = FALSE;
}
else
{
user_seq_of_ordered_steps++; // This variable is needed because I want to generate only theree sequences of impulses
if(user_seq_of_ordered_steps < 3)
{
htim1.Instance->RCR = ++user_no_of_steps; // This value is initially 0
htim1.Instance->EGR = TIM_EGR_UG;
// Make this flag TRUE to enter again the interrupt to update the TIM1 registers
flag_update_event = TRUE;
/* Enable the Peripheral */
__HAL_TIM_ENABLE(&htim1);
}
}
/* USER CODE BEGIN TIM1_UP_IRQn 1 */
/* USER CODE END TIM1_UP_IRQn 1 */
}