How the H750 kernel is powered using an external power supply
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-05-10 1:29 AM
When using the STM32H750VBT6, I supplied around 1.37-1.4 supply voltage to the external pins VCAP1 and VCAP2,the project was configured as an external power supply using cubemx software.HAL_PWREx_ConfigSupply(PWR_EXTERNAL_SOURCE_SUPPLY); is used in the program.Frequency automatically configured to 480 MHz via cubemx (internal clock source).
According to the manual said burned into the power-off restart, and then to be effective, after the start may not be able to recognize the chip can not be debugged, good luck may be debugging, but run for a while will enter the Hardware Error Interrupt Function in the HardFault_Handler().How to solve this problem.
Solved! Go to Solution.
- Labels:
-
STM32H7 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-05-10 1:55 AM
>supplied around 1.37-1.4
"around" is not adequate definition here ; :)
+
this is core supply , maybe 200mA needed; so R48/49 = 0.
And Vcap low noise, low impedance source !
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-05-10 1:55 AM
>supplied around 1.37-1.4
"around" is not adequate definition here ; :)
+
this is core supply , maybe 200mA needed; so R48/49 = 0.
And Vcap low noise, low impedance source !
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-05-10 2:30 AM
Voltage fixed at 1.375V,Do you mean to use 0R resistors for R48 and R49?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-05-10 3:04 AM
切换到 0R 解决了它,谢谢