2025-04-06 9:06 AM
Dear Community,
I’m currently developing with the STSPIN32G4, but I’m encountering some difficulties related to flashing and powering the chip.
Below is a summary of my setup and the issues I’m facing:
I'm using ST-Link V2 with the following connections:
SWDIO, SWCLK, GND, and VCC
I would like to use an external 3.3V power source to power the STSPIN32G4
Case 1: Powered by ST-Link V2 (VCC connected)
Case 2: Powered by external 3.3V
Any insights or suggestions would be greatly appreciated. Thanks in advance for your support!
Best regards,