2023-06-01 10:08 PM
2023-06-01 11:38 PM
Look just after the TIMx_SMCR description in individual timer chapters in R0390, in "TIMx internal trigger connections" tables.
It should be the same as in 'F407, which I have in a single table here. However, RM takes precedence, as usually.
AN4640 is what "Interconnections" is in other STM32 RMs; but sadly, it won't go to sufficient detail (as those chapters won't either).
JW