2022-04-02 2:40 AM
I am new to STM32s programing in general and am trying to create some simple libraries, altough I have no idea how I would make it so that I can write it in a way, that needed ports and pins are given in function inputs. For example: int HCSR04_Distance(___, ___); HCSR04 is a distance sensor, how do I input the port and pin on the empty lines?
Thank you in advance and have a nice day
2022-04-02 3:53 AM
There are many ways to approach this, depending on what do you exactly want to achieve (execution speed, written code size and readability, etc.) For example:
int HCSR04_Distance(GPIO_TypeDef * pGPIO, uint32_t pin) {
_Bool pinState;
// if you need to read the pin
pinState = (_Bool)(pGPIO->IDR & (1 << pin));
// if you need to change the pin from digital input to digital output
// beware if used in interrupts, this is non-atomic
pGPIO->MODER = (pGPIO->MODER & ~(0b11 << (2 * pin))) | (0b01 << (2 * pin));
// if you need to set the pin
pGPIO->BSRR = 1 << pin;
// if you need to clear the pin
pGPIO->BSRR = 1 << (pin + 16);
return pinState;
}
int main(void) {
// usage, for example for PB4:
previousPinState = HCSR04_Distance(GPIOB, 4);
}
// --- an alternative: define a structure for the pin
typedef struct {
GPIO_TypeDef * pGPIO;
uint32_t pin;
} gpio_pin_t;
int HCSR04_Distance(gpio_pin_t p) {
_Bool pinState;
// if you need to read the pin
pinState = (_Bool)(p.GPIO->IDR & (1 << p.pin));
return pinState;
}
const gpio_pin_t HCSR04_Pin = {.pGPIO = GPIOB, .pin = 4};
int main(void) {
previousPinState = HCSR04_Distance(HCSR04_Pin);
}JW
2022-04-02 4:06 AM
I see. This is perfect, thank you!