2022-01-11 1:31 PM
2022-01-11 3:28 PM
Set up a timer to trigger a periodic DMA transfer. Set up that DMA stream to transfer between an array to GPIOx->BSRR. Only works if all pins are on the same port. Frequency will be limited so something on the order of 10 MHz.
2022-01-11 3:28 PM
Set up a timer to trigger a periodic DMA transfer. Set up that DMA stream to transfer between an array to GPIOx->BSRR. Only works if all pins are on the same port. Frequency will be limited so something on the order of 10 MHz.
2022-01-11 4:48 PM
Want a 16-bit write to ODR, or 32-bit to BSRR, would suggest the latter as you can pick the pins you want to leave an those you want to touch.
Seem to recall the GPIO is on AHB4, so perhaps SRAM4 via BDMA
I built an example the other week or two ago, and there was a thread
2022-01-14 11:34 AM
@Community member
I looked for a minute on your profile and couldn't find that thread. Any chance you might be able to link it here?
After reading up on the H7 series, its looking like I have a few things I will need to do because of the problems with the M7's d-cache having issues with the DMA. I don't want to globally disable d-cache, as I will be doing more than just DMA transfers here, but yeah. The rabbit hole goes deeper on...
@TDK
Your idea is kind of similar to what my team and I had hoped to do for this project initially, but we are running in to all kinds of strange errors with the H7 series that were unexpected. Ethernet and DMA alike seem to have little quirks in memory configuration and such that make this more complicated than necessary.
Thanks for your help all!
2022-01-17 8:04 PM
Simple way:
if (HAL_DMA_Start_IT(htim->hdma[TIM_DMA_ID_UPDATE],
(uint32_t)pData,
(uint32_t)&htim->Instance->ARR, // before
Length) != HAL_OK)
if (HAL_DMA_Start_IT(htim->hdma[TIM_DMA_ID_UPDATE],
(uint32_t)pData,
(uint32_t)&GPIOA->ODR, // after
Length) != HAL_OK)
Use MY_TIM_Base_Start_DMA to start timer before main loop.
Also can be used with input capture + dma to provide external clock for data output, then you alter HAL_TIM_IC_Start_DMA(). Copy-paste it to user code, rename to MY_TIM_IC_Start_DMA and alter destination to GPIO register
2022-01-17 9:09 PM
Any chance to see a list of "strange errors" you team is running into?