cancel
Showing results for 
Search instead for 
Did you mean: 

How do I distinguish between 405 and 407 processor in software? The signature is the same.

Peter Mather
Associate III
Posted on December 06, 2017 at 18:29

I'm writing code that can run on both 405 and 407 processors but the device signature is the same for both. How can my code tell which it is running on?

Thanks

2 REPLIES 2
Posted on December 06, 2017 at 22:41

You can't.

Use some different way - differences in externally connected hardware, your own 'signature' programmed during initial tests...

JW

Posted on December 06, 2017 at 22:49

What features are you using on one and not the other? How is the circuit they are used in different? Ethernet? check presence of PHY? Put a serial# in OTP.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..