STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 I/O port characteristics

Posted on May 23, 2018 at 11:32Hello, I�m struggling understanding the I/O static characteristics for the STM32H7 devices.I think that below 0.3xVdd a normal input is low and above 0.7xVdd it is high. But what is the meaning of the red marked lines?...

0690X00000604h9QAA.jpg

P-L496G-CELL01 - price & availability?

Posted on February 14, 2018 at 20:15Hi,Does anybody know when this module will be available and how will be priced?http://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mcu-eval-tools/stm32-mcu-eval-tools/stm32-mcu-d...

Resolved! STM32L4R5ZI reset issue.

Posted on May 31, 2018 at 15:48Archive addition leading to Reset.Now its failing in SystemClock_Config.And entering to WWDG_IRQHandler() at startup_stm32l4r5xx.s:132 0x8009dc0Failing at RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; RCC_OscInitTypeDef ...

CubeMX F4 LL GPDSC code generation issues

Posted on December 14, 2017 at 09:26Hi,I've run into some problems when generating and then importing a GPDSC project when using LL drivers only.Environment: Visual Studio 2017 + VisualGDB (includes STM32CubeMX GPDSC importer)STM32CubeMX V4.23STM32C...

parsec by Associate III
  • 1211 Views
  • 1 replies
  • 0 kudos

X-CUBE-MEMSMIC with 4 channel microphone problem

Posted on October 26, 2017 at 16:51hi, I have  a stm32l476 necleo-64 board and CCA02M1 extension board. I want to modify the the Microphones_Streaming example. and I want to use it to record 4 channel microphone and with 48000Hz sample rate. and I j...

0690X00000608f2QAA.png 0690X00000608lOQAQ.png 0690X00000608jJQAQ.png

STM CubeMX F103 RTC settings problem

Posted on December 17, 2017 at 23:24Hi,In STMCubeMX for stm32F103CBT6, i can not set the time of RTC more than 12 !!! it shows:'HoursHours must be between 1 and 12.Diagnostic:Hour Format is 12H 'but in the Alaram value field, it can be 0-23 !!! :'Ho...

STM32F042 Bootloader via CAN BUS

Posted on June 01, 2018 at 11:21Hi all,  As a title, can I use CAN Bus protocol to update my firmware with STM32F042K6T6 ? Because our product just has CAN Bus protocol and no others. thanks a lot.

STM32L152: Connect the COMP2 output to the IO port

Posted on June 01, 2018 at 11:22I want to connect the COMP2 output to the external circuit. I know the output can be redirected to the IC channel of some timers.and I tried to use TIM2_IC4 to get the output of COMP2 but failed.Is it possible to impl...

lei yue by Associate
  • 659 Views
  • 0 replies
  • 0 kudos