cancel
Showing results for 
Search instead for 
Did you mean: 

How can we do the simple UART for the STM32H745I-DISCOVERY board using the MDK-ARM?

sredd.3
Associate II

I am using stm32h745i-discovry board as my development in the arm keil. Here I need the uart communication . could you please send me the example code for this.

3 REPLIES 3

https://community.st.com/s/question/0D53W00001UYJq2SAH/how-can-i-receive-the-data-through-the-uart-in-the-stm32h745i

Which UART, what pins?

Should be some examples under CubeH7, with Keil project files

Need something specific, accept PayPal and Venmo..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Piranha
Chief II

You were given the example, but you haven't even commented anything about it and are asking for example again. And the internet is full of examples...

https://github.com/MaJerle/stm32-usart-uart-dma-rx-tx

Asking the same question million times will not change the reality - either you learn it or you hire someone who can do it!

Hi Piranha,

I hope this is not the way to deliver the answer Piranha...

I asked the same question again because I thought whether you guys can understand my words or not in the previous question. I did not get more information with that info given by the team...that is why I mentioned very simply and sent it back...

thanks for your time for typing the unnecessary words in the above reply.

thank you again.